I2C Motor Driver

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
Gunther
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Mon Feb 27, 2012 4:24 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Grove - I2C Motor Driver
Contact:

I2C Motor Driver

Post by Gunther » Mon Feb 27, 2012 4:38 am

Hello, I want to hook the Motor Driver up to an Arduino to control it. I saw the code on the wiki but I am unsure what pins between the two devices should be connected as they were when the sample code was written. (sample code from http://www.seeedstudio.com/wiki/Grove_- ... tor_Driver)

schmron
Elementary-1
Elementary-1
Posts: 145
Joined: Mon Dec 05, 2011 6:12 am

Re: I2C Motor Driver

Post by schmron » Mon Feb 27, 2012 7:09 am

Just connect it to the I2C interface on your Arduino:
http://www.arduino.cc/en/Reference/Wire

But its better to use one of the I2C connectors on a Grove Base Shield.
http://www.seeedstudio.com/depot/grove- ... th=132_134
Best regards from Vienna/Austria
Rony

Post Reply