Compatibility 3-Axis Compass module v1.0b and SeeeduinoV3.0

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
Gennady
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Feb 22, 2012 6:28 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: 3-axis Compass

Compatibility 3-Axis Compass module v1.0b and SeeeduinoV3.0

Post by Gennady » Wed Feb 22, 2012 6:55 am

Please help make the right choice. I want to purchase 3-Axis Compass module v1.0b SKU SEN12753P and Seeeduino V3.0 (Atmega 328P) SKU ARD128D2P.

The first question is - do I need any additional cables and boards to connect these devices?

The second question - whether enough of the program is a compass, which is located at http://www.seeedstudio.com/wiki/index.p ... pass_v1.0b (code in file Compass.zip), so that I could see on my PC work a compass as shown on the same page?

Thanks!

yuriq
Elementary-3
Elementary-3
Posts: 383
Joined: Wed Dec 07, 2011 5:33 pm

Re: Compatibility 3-Axis Compass module v1.0b and Seeeduino

Post by yuriq » Wed Feb 22, 2012 10:52 am

Dear customer,

1. Yes, you should use Base shield via Grove wire to connect with Seeeduino.
http://www.seeedstudio.com/depot/grove- ... th=132_134
Or you also can connect jumper wire by yourself to use softserial I/O port with compass.

2.Yes,follow WIKI you can do that.

Gennady
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Feb 22, 2012 6:28 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: 3-axis Compass

Re: Compatibility 3-Axis Compass module v1.0b and Seeeduino

Post by Gennady » Wed Feb 22, 2012 3:28 pm

Thanks!

Post Reply