My i2c motor driver does not work, I want to change the firmware but I have not enough information, I downloaded the .hex file but not as upload it to the board.
Can you help?
thanks
It worked fine at first but it seems that is locked, now all LEDs remain lit and does not work, I have no other i2c device to test the i2c bus, the motor driver may be blocking the bus i2c. I have to buy a grove rtc to try. I dont know if there is a way to know if the motor driver works, to make it respond messages
It worked fine at first, all connection are ok. I am using a shield with an arduino and the i2c Motor Driver. I tried the code of the link but it does not work, Motor Driver keep all the LEDs on.
I would like to send something to the Motor Driver and this reply through i2c but i am not sure if it is possible.
I’m trying to flash the frimware of my I2C motor driver but I’m struggling with the AVR programmer. I bought the AVRISP programmer from seeedstudio.
Please see enclosed a picture which shows how I connect to the board.
A had the similar problem. It was wrong pinout written at the board. But my board looks quite different (may be I have an old version of it).
Try to look at atmega8 datasheet, and check wheather the MISO, MOSI and SCK pins of controller connected to the proper pins of the socket.
So is the actual SOURCE CODE of the firmware somewhere online? The wiki link File:Grove-I2C Motor Driver firmware.zip seems to only have a file with hex values in it, no source code.
I want to know if I can extend the firmware so it can work with dc motors with encoders.
I’m also having trouble getting this board up and running. When I connect power all 4 direction and the power led go on. Doesn’t matter whether I2C is connected or not. Any ideas? How to check whether it’s a DOA?
Also, my board has v1.0 printed on the back. Does that mean it’s an outdated version?
And lastly, anyone got stepper motor code for it? That’s what I bought it for but the sample code is only for DC motors.
I’m trying to operate it from an Arduino Uno with several other devices on the I2C bus.
Looks like an outdated board indeed, it doesn’t have the address dipswitch… Any know if other things have changed as well?
Apart from that, I was able to run the DC motor sample code successfully. I’m now trying to integrate it with my main application which involves other devices on the bus (ADXL345, MPR121). Now all power and direction led’s light again and the board doesn’t respond. Is this a signal for a certain error state that can help me debugging?
Still would like stepper motor action instead of DC, too.
I’ll just keep logging my progress here. Perhaps it’ll help someone at some point…
Turns out my older version board has address 0x28 instead of the current one’s 0x0f.
Looks like my board is the same as the one in the link posted earlier in this thread: salviusrobot.blogspot.nl/2012/03/grove-i2c-motor-driver-setup-and.html (forum doesn’t let me post links)
I found a basic stepper library for the Grove/Twig I2C driver here: github.com/mariolukas/TwigMotor-Library
Mind you, serial addresses are set for the older version boards. Change them for newer versions.
The code is also pre-arduino-1.0. I’ve patched 2 files in the repository for 1.0+ compatibility.
Actually the stepper mode is really not complicated, just badly documented in the wiki. What you need to do is set the ‘channel set’ / ‘direction set’ registry alternatingly for your motor’s 2/4/6/8 steps.
When I got TwigMotor working I started merging its I2C functionality with the AccelStepper library: open.com.au/mikem/arduino/Ac … index.html
It’s a great arduino stepper library with non-blocking code, acceleration/deceleration, etc.
I now have an alpha version of AccelStepper with an additional mode for I2C control of the Grove board (and potentially other I2C stepper drivers). I’ll publish it once it’s cleaned and tested.