Tutorial: Reading Water Flow rate with Water Flow Sensor

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: violet, jessie

jim85133
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Jul 31, 2015 11:55 am

Re: Tutorial: Reading Water Flow rate with Water Flow Sensor

Post by jim85133 » Fri Jul 31, 2015 12:00 pm

What distance can you send the signal from the flowmeter? How do you determine this? If the yellow signal wire to the seeeduino is 50 yards, would it still read properly on pin 2?

ari4
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Jun 04, 2014 5:50 pm

Re: Tutorial: Reading Water Flow rate with Water Flow Sensor

Post by ari4 » Sun Sep 13, 2015 3:22 pm

Hello,
I have a flow meter and have everything wired up to an arduino uno. the signal is coming in at digital port 4. my problem is that when i power the arduino and upload the code, without having the pump on i get values like 520, 512 etc. I am testing the system with a small fish tank pump and when i turn it on, i now get values like 240, 304, 248 etc.

Three questions,
1)why am i getting 520 when there is no water flowing through the meter? I would expect this to be zero not a value like 520
2)Why do values vary so much on every sample? i can see 224, 280, 356, 404, 232,288 etc when the pump is just pumping the same amount more or less.
3)In the sample code the equation is

Calc = (NbTopsFan * 60 / 4.5); // (Pulse frequency x 60) / 4.5Q, = flow rate in L/hour

but in the comments above, it seems that the 4.5 suppose to be 7.5. Which one is correct?

Thanks

piyush17395
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Mar 05, 2016 12:24 pm

Re: Tutorial: Reading Water Flow rate with Water Flow Sensor

Post by piyush17395 » Sat Mar 05, 2016 12:26 pm

I'm trying to interface the sensor with Arm7.
Can you tell me what pin2 corresponds to so that i can interface it with ARM7.

sfcable4seo
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Mon Apr 09, 2018 2:55 pm
Location: USA
Contact:

Re: Tutorial: Reading Water Flow rate with Water Flow Sensor

Post by sfcable4seo » Mon Apr 09, 2018 3:00 pm

nice Reading Water Flow rate with Water Flow Sensor

Post Reply