Seeeduino-Film now what?

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Nonya-Biz
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Tue Aug 10, 2010 7:22 am

Seeeduino-Film now what?

Post by Nonya-Biz » Tue Aug 10, 2010 8:05 am

i ordered one of the film boards, but it didn't come with a usb programer. now what?

User avatar
Albert.Miao
Elementary-2
Elementary-2
Posts: 250
Joined: Sun Nov 23, 2008 9:23 am

Re: Seeeduino-Film now what?

Post by Albert.Miao » Wed Aug 11, 2010 8:41 pm

USB to Uart Needed.
http://www.seeedstudio.com/depot/uartsb ... th=104_109
The new version UartSB v3 will available soon.
Thanks
Albert

Nonya-Biz
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Tue Aug 10, 2010 7:22 am

Re: Seeeduino-Film now what?

Post by Nonya-Biz » Thu Aug 12, 2010 1:44 pm

why is there no programer included?

Nonya-Biz
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Tue Aug 10, 2010 7:22 am

Re: Seeeduino-Film now what?

Post by Nonya-Biz » Sun Aug 15, 2010 2:12 pm

someone should probly mention that next time you send out mass e-mails. even a seporate programing breakout would have been nice.

maxwell
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Nov 11, 2010 8:22 pm

Re: Seeeduino-Film now what?

Post by maxwell » Thu Nov 11, 2010 8:35 pm

Hello!

I also ordered a film and wanted to upload a sketch via the arduino dev environment onto the board.
Surprisingly :shock: nothing happend and i got an error when uploading the code.

I guess i have to manually flash the bootloader onto the chips?
If so, how can I accomplish that?

Arduino related things I've got:
Arduino Lilypad + FTDI Basic Breakout - 3.3V (sparkf...)
Arduino Film

Thanks in advance!

drhenrich
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Nov 12, 2010 1:16 am

Re: Seeeduino-Film now what?

Post by drhenrich » Fri Nov 12, 2010 1:36 am

Hi,
I received the beta version of Seeeduino-film together with the Motion-Frame and managed to program it with the UartSBee V3.1 with the examples provided. In order to compile with Arduino 21 I had to remove the SPI from the libraries folder and change from <Spi.h> to "Spi.h" (in all the files where it applies) choosing 8Mhz/AtMega168. I ran data record, data access and access of the accelerometer. Temp/Altitude is working but the accelerometer returns only zero. Is this due to a bug in the betafilmversion or is there an error in the acc-code ??? (I'm expecting the final Seeeduino-film, so I'll check it in a couple of days....)

roadknightlabs
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri Dec 03, 2010 8:08 am

Re: Seeeduino-Film now what?

Post by roadknightlabs » Sat Dec 11, 2010 3:15 pm

maxwell wrote:Hello!

I also ordered a film and wanted to upload a sketch via the arduino dev environment onto the board.
Surprisingly :shock: nothing happend and i got an error when uploading the code.

I guess i have to manually flash the bootloader onto the chips?
If so, how can I accomplish that?

Arduino related things I've got:
Arduino Lilypad + FTDI Basic Breakout - 3.3V (sparkf...)
Arduino Film

Thanks in advance!
Hi Maxwell,
Have you received your board yet ?
Have you been able to upload a sketch to it ?
(If yes) How did you do that ?

maxwell
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Nov 11, 2010 8:22 pm

Re: Seeeduino-Film now what?

Post by maxwell » Sat Dec 11, 2010 4:47 pm

Hello!

Yes I have ordered 2 (beta) boards which I already received.

Uploading Sketches does not work.
My setup:
PC -> FTDI basic breakout 3.3V from sparkfun -> film.

The film seems to be the problem because uploading sketches to other arduinos works without any problems.

As mentioned in early posts my guess is that there is no arduino-preinstalled-bootloader on the film.
Sadly I haven't found a way burn a bootloader without special hardware/programmers.

I'm just waiting for anyone to confirm the there is no bootloader on the chips.

Thanks in advance!

roadknightlabs
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri Dec 03, 2010 8:08 am

Re: Seeeduino-Film now what?

Post by roadknightlabs » Sat Dec 11, 2010 6:00 pm

maxwell wrote:Hello!

Yes I have ordered 2 (beta) boards which I already received.

Uploading Sketches does not work.
My setup:
PC -> FTDI basic breakout 3.3V from sparkfun -> film.

The film seems to be the problem because uploading sketches to other arduinos works without any problems.

As mentioned in early posts my guess is that there is no arduino-preinstalled-bootloader on the film.
Sadly I haven't found a way burn a bootloader without special hardware/programmers.
Alas, this also matches my experience.
I'm wondering how we're supposed to get a bootloader on the devices if normal 5V ISP programmers won't work on these boards.

irgendwie
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Thu Nov 18, 2010 2:40 am

Re: Seeeduino-Film now what?

Post by irgendwie » Sun Dec 12, 2010 5:34 am

I was able to upload a program with this setup.
I'm using the FTDI 3.3V basic
http://www.sparkfun.com/products/8772
What is confusing is that the middle section and the outer section of the film have two areas that are similar (VCC, TX, RX). Make sure to use the middle area.
FTDI TXO -> RX FILM
FTDI RXI -> TX FILM
photo(2).JPG
photo(2).JPG (46.6 KiB) Viewed 4976 times
loaded this program

/*
Blink
Turns on an LED on for one second, then off for one second, repeatedly.

This example code is in the public domain.
*/

void setup() {
// initialize the digital pin as an output.
// Pin 13 has an LED connected on most Arduino boards:
pinMode(8, OUTPUT);
}

void loop() {
digitalWrite(8, HIGH); // set the LED on
delay(4000); // wait for a second
digitalWrite(8, LOW); // set the LED off
delay(1000); // wait for a second
}

Post Reply