Arduino Yun Compatibility

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: violet, salmanfarisvp

Post Reply
cameron.watson
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Thu Nov 08, 2018 3:05 pm

Arduino Yun Compatibility

Post by cameron.watson » Thu Nov 08, 2018 3:12 pm

I am looking for advice on how compatible the SeeeduinoCloud is with the ArduinoYun.

I have a custom board that a friend of my developed that plugged into the Arduino Yun. The Arduino has since died and I purchased a SeeeduinoCloud as a replacement. The problem is when I connect a battery pack to the custom board, the Seeeduino does not power up like the Yun did.

Just wondering if there are any differences between power pins in the Seeeduino???

As a side note, the custom board works when powered from USB, but I require 12V so powering via USB is not an option.

Excuse me for lack to technical knowledge. I am just trying to get the device to work like it previously did.

bill.yu
Elementary-4
Elementary-4
Posts: 400
Joined: Mon Apr 02, 2018 11:05 am

Re: Arduino Yun Compatibility

Post by bill.yu » Fri Nov 09, 2018 7:18 pm

Hi there,

both of them use ATmega32u4 and the Atheros AR9331. they use the standard arduino pinout, 5v working voltage.

do you mind posting about the whole hardware setup?

or can you power the seeeduino cloud through usb cable individually? here is the wiki about http://wiki.seeedstudio.com/Seeeduino_Cloud/.

you can download the blink program and see if it works.
http://wiki.seeedstudio.com/Seeeduino_C ... ng-started

thanks.

Post Reply