ISP programming in Hercules 4WD robot controller

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: violet, jessie

Post Reply
vishwanathm28
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Oct 29, 2018 5:24 pm

ISP programming in Hercules 4WD robot controller

Post by vishwanathm28 » Mon Oct 29, 2018 5:33 pm

Hi,

Can i program the Hercules 4WD robot controller using the ICSP interface using any ISP programmer?
http://wiki.seeedstudio.com/Hercules_Du ... ontroller/

Is so can i use arduino UNO as ISP or arduinoISP ?


Thanks

bill.yu
Elementary-3
Elementary-3
Posts: 358
Joined: Mon Apr 02, 2018 11:05 am

Re: ISP programming in Hercules 4WD robot controller

Post by bill.yu » Tue Oct 30, 2018 6:10 pm

Hi there

Yes, you can, when you use the icsp to program the board, the bootloader will be flashed and then you can not use the rx/tx to program it again. if you want to program through rx/tx, you have to flash the bootloader again. thanks.

Post Reply