Is that possible to connect GSR sensor to the servo?

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: violet, jessie

Post Reply
573587188
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Jun 19, 2018 7:19 am

Is that possible to connect GSR sensor to the servo?

Post by 573587188 » Mon Jul 16, 2018 8:21 pm

Is that possible to connect GSR sensor to the servo? I would like to use the output of GSR sensor connected to a 6-channel Maestro servo controller to control the position of one of my standard RC servos.

hong.jiang
Staff
Staff
Posts: 200
Joined: Tue Apr 17, 2018 11:03 am

Re: Is that possible to connect GSR sensor to the servo?

Post by hong.jiang » Tue Jul 17, 2018 10:01 am

Hi, the GSR sensor output is around 200~300. ADC is 10bits. So it is around 20%~30%VCC. if VCC is 5v, it will be 1~1.5V. thanks.

Seeed techsupport team
Bill

Post Reply