FAT32 and stalker

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
rich
Elementary-1
Elementary-1
Posts: 171
Joined: Wed Oct 21, 2009 12:24 pm

FAT32 and stalker

Post by rich » Fri Jun 04, 2010 2:48 pm

I have been trying to get a FAT 32 implementation so I can use the only card I have, a 16G card, to work with a gps library for time and position. The goal being position and temperature logging to a text file or set of files that I can read on other systems. Unfortunately all my attempts to combine implementations FAT32 and NEMA parsing do not fit. I can get within 1k, but no closer. Has anyone succeeded in doing this or a similar task? What libraries did you use?

User avatar
min0n
Pre-kindergarten
Pre-kindergarten
Posts: 9
Joined: Mon Mar 15, 2010 11:01 pm

Re: FAT32 and stalker

Post by min0n » Sat Jun 05, 2010 9:21 pm

I use :
http://code.google.com/p/fat16lib/
and
http://code.google.com/p/sdfatlib/
from Bill.Greiman with arduino mega... and work ok.
i havent tested on stalker..
if you test it, please post a comment with results.

FreeZinG

Re: FAT32 and stalker

Post by FreeZinG » Mon Jun 07, 2010 10:22 pm

If you find a code that using SPI interface and support , that the stalker can support the FAT32 either . Now we provide the code that is a not a fully file system and just a filelogger demo , so it just support FAT16 and appending data into a existent file.

rich
Elementary-1
Elementary-1
Posts: 171
Joined: Wed Oct 21, 2009 12:24 pm

Re: FAT32 and stalker

Post by rich » Wed Jun 16, 2010 1:17 pm

I have gotten to within 1k of fitting, but no better :-( I hate 168s...

User avatar
esp
Elementary-3
Elementary-3
Posts: 361
Joined: Fri Aug 22, 2008 5:45 pm

Re: FAT32 and stalker

Post by esp » Fri Jun 18, 2010 3:25 pm

Stalker with 168 will get extincted ...soon.

Post Reply