Seeeduino and Seeeduino Cloud USB power bank

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: violet, jessie

Post Reply
ivanlomy
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Mar 28, 2018 6:46 pm

Seeeduino and Seeeduino Cloud USB power bank

Post by ivanlomy » Tue Apr 17, 2018 10:26 pm

Really love to power up my Seeeduino and Seeeduino Cloud by portable PowerBank.
The spec of my USB PowerBank is:
10000mAh 3.85V ( 38.5Wh )
input 5.0V2.0A 9V/12V18W
output 5.1V2.0A 9V/12V12W

for this spec, it is safe to power up my boards? for long operation hrs (1 months) also safe?
If I use other PowerBank with 2.4A output, also safe?
Thx
Ivan

bill.yu
Elementary-2
Elementary-2
Posts: 297
Joined: Mon Apr 02, 2018 11:05 am

Re: Seeeduino and Seeeduino Cloud USB power bank

Post by bill.yu » Tue Jun 05, 2018 4:18 pm

Hi Ivan, For the current and voltage, both of them works with seeeduino. For the operation time, the power consumption depends on the sensors as well. We suggest use https://www.seeedstudio.com/USB-Current ... -1925.html to detect the power consumption. thanks.


Seeed techsupport team
Bill

Post Reply