Seedstudio Lotus external power supply

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
mail28
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Jan 16, 2016 8:53 pm

Seedstudio Lotus external power supply

Post by mail28 » Sat Jan 16, 2016 8:57 pm

Hi everyone,

I bought a Seedstudio Lotus board and a Grove I2C Motor Driver to make my first robot. So, my question is : how can i supply external power to my Lotus board ? I have a DFRobot Turtle mobile platform with five 1.5V batteries slots to plug with the Motor Driver board, but I don't know how to connect this power supply to my arduino board.

Thanks in advance !

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: Seedstudio Lotus external power supply

Post by kavi » Tue Jan 19, 2016 5:45 pm

Hi,

Connect the battery to Seeeduino lotus using jumper wires as follows

Code: Select all

Lotus    Battery
5V-------->4.5~5V
GND------>GND
Thanks and Regards

sbianchina
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed May 04, 2016 11:56 pm

Re: Seedstudio Lotus external power supply

Post by sbianchina » Thu May 05, 2016 12:10 am

Hello

is there a voltage regulator behind the LOTUS 5V PIN (can I plug a 9V battery) ?
what is the maximum and minimum amperage supported ?

2d question : Can I connect the USB cable to a battery (same questions is there a power regulator that allows us to send more than 5V and what is the amperage supported) ?

Thank you for your help
SB

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: Seedstudio Lotus external power supply

Post by kavi » Thu May 05, 2016 3:38 pm

Hello,

1. 9V battery cannot be connected to the 5v pin of the Seeeduino Lotus.There is a voltage regulator connected to lotus 5v pin but it cannot be supplied more than 5v.The maximum ampere rating is 800mA.The voltage regulator converts 5V to 3.3V.
So the maximum voltage that can be applied is 5v.

2.It is possible to connect the battery (5v only and not more than that)to the USB.Please check the polarity before connecting them.

Thanks and Regards

Post Reply