Page 1 of 1

Stalker V3 compatibility with Same box as V2.3?

Posted: Mon Dec 22, 2014 2:21 pm
by mholler
Does the Stalker V3 which has a different board shape, without the corner cutouts and a little shorter than the V2.3 , fit in the plastic box you have been selling for V2.3?

Re: Stalker V3 compatibility with Same box as V2.3?

Posted: Mon Dec 22, 2014 6:24 pm
by shaopeng.zhang
mholler wrote:Does the Stalker V3 which has a different board shape, without the corner cutouts and a little shorter than the V2.3 , fit in the plastic box you have been selling for V2.3?
Hi mholler,

Thanks for your question!
The size of Stalker V3 is 86.74mm x 60.96mm, and it can be put inside of this plastic enclosure for V2.3: http://www.seeedstudio.com/depot/Seeedu ... Path=55_60
Thanks!

Re: Stalker V3 compatibility with Same box as V2.3?

Posted: Tue Jan 06, 2015 5:10 pm
by mail26
Is only the case compatible or also the mounting holes?

Re: Stalker V3 compatibility with Same box as V2.3?

Posted: Mon Jan 12, 2015 11:51 am
by Jacket Chen
mail26 wrote:Is only the case compatible or also the mounting holes?
Both different. V3 is smaller than v2.3, so it can plugged into the box of v2.3. But we may make a new box for v3 alone.

Jacket