Stalker V3 compatibility with Same box as V2.3?

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
mholler
Pre-kindergarten
Pre-kindergarten
Posts: 11
Joined: Thu Dec 18, 2014 9:35 pm

Stalker V3 compatibility with Same box as V2.3?

Post by mholler » Mon Dec 22, 2014 2:21 pm

Does the Stalker V3 which has a different board shape, without the corner cutouts and a little shorter than the V2.3 , fit in the plastic box you have been selling for V2.3?

shaopeng.zhang
Staff
Staff
Posts: 50
Joined: Sun Apr 27, 2014 7:49 pm

Re: Stalker V3 compatibility with Same box as V2.3?

Post by shaopeng.zhang » Mon Dec 22, 2014 6:24 pm

mholler wrote:Does the Stalker V3 which has a different board shape, without the corner cutouts and a little shorter than the V2.3 , fit in the plastic box you have been selling for V2.3?
Hi mholler,

Thanks for your question!
The size of Stalker V3 is 86.74mm x 60.96mm, and it can be put inside of this plastic enclosure for V2.3: http://www.seeedstudio.com/depot/Seeedu ... Path=55_60
Thanks!

mail26
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Tue Jan 06, 2015 5:08 pm

Re: Stalker V3 compatibility with Same box as V2.3?

Post by mail26 » Tue Jan 06, 2015 5:10 pm

Is only the case compatible or also the mounting holes?

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Stalker V3 compatibility with Same box as V2.3?

Post by Jacket Chen » Mon Jan 12, 2015 11:51 am

mail26 wrote:Is only the case compatible or also the mounting holes?
Both different. V3 is smaller than v2.3, so it can plugged into the box of v2.3. But we may make a new box for v3 alone.

Jacket
Love little, love long.

Post Reply