new Seeeduino ADK v.0 not working

Hello,



I won a Seeeduino ADK v1.0 today at the Maker Faire in Hannover.

Now I’m wondering how to start things up.



It’s connected via Micro USB to my PC.

If I try to select it’s port in the Arduino IDE or UECIDE, it’s not shown up.

Trying to install the Arduino drivers didn’t show any effect.

Even in the device manager of Windows the Seeeduino is not listed.

Same problem on Linux (Manjaro).



What else could be a problem?

I didn’t find any drivers for the mentioned board.

Is it outdated and not supported anymore?

I got the board withing the original package.



Thanks for everyone’s help,

Jakob

HI Jakob~



Please make sure the usb cable is 4 wires, which can transfer data. You can refer to below link for detail operation. thanks.



http://wiki.seeedstudio.com/Seeeduino_ADK_Main_Board/