Error: Network initialize timeout in Wio LTE Cat M1/NB-IoT Tracker

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
ateeque.rahman1
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri May 17, 2019 5:11 pm

Error: Network initialize timeout in Wio LTE Cat M1/NB-IoT Tracker

Post by ateeque.rahman1 » Fri May 17, 2019 5:28 pm

I have recently bought Wio LTE Cat M1/NB-IoT Tracker. i worked on Grove sensors, GNSS and on board RGB LED all are working fine.
but when i insert the 4G vodafone SIM and run the RSSI example code, Ublox gets powered on and also SIM is detected whereas Network initialization is failed.
Do I need to have LTE CAT M1 enabled for my SIM card ?? or is it necessary that the LTE Cat M1 network is implimented in my area of testing?
I am located in Bengaluru, India, 560001

Serial data from Unit:
................................................................................
.......................................[ERROR] Network initialize timeout.
................................................................................
.......................................[ERROR] Network initialize timeout.
................................................................................
.......................................[ERROR] Network initialize timeout.
................................................................................
.......................................[ERROR] Network initialize timeout.
................................................................................
.......................................[ERROR] Network initialize timeout.
................................................................................
.......................................[ERROR] Network initialize timeout.

hope to get the reply soon, Thanks in advance

User avatar
salmanfarisvp
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Sun May 20, 2018 2:02 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Linklt One , BeagleBone Green , ReSpaker
Contact:

Re: Error: Network initialize timeout in Wio LTE Cat M1/NB-IoT Tracker

Post by salmanfarisvp » Wed May 22, 2019 4:54 pm

Hi Rahman , Can you please share your sketch , to get more deatils.

Thanks .

ateeque.rahman1
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri May 17, 2019 5:11 pm

Re: Error: Network initialize timeout in Wio LTE Cat M1/NB-IoT Tracker

Post by ateeque.rahman1 » Tue May 28, 2019 1:16 pm

Below is the RSSI Example code.
=======================================================================================================
#include <ublox_sara_r4.h>
#include <UART_Interface.h>

Ublox_sara_r4 ublox = Ublox_sara_r4();

void setup() {

SerialDebug.println("Begin...");
ublox.powerOn();
SerialDebug.print("Waitting for module to alvie...");
while(false == ublox.isAlive()){
SerialDebug.print(".");
delay(100);
}

while(!ublox.network_Init(30000)) { // changed t0 180 i.e nearly 3 mins
Log_error("Network initialize timeout.");
}
Log_info("APN: " + String(ublox._apn));
Log_info("Local IP: " + String(ublox._str_ip));
Log_info("Operator: " + String(ublox._operator));
Log_info("Network attached.");
}

void loop() {
int signal;
if(ublox.getSignalStrength(&signal)) {
SerialDebug.print("RSSI: ");
SerialDebug.println(signal, DEC);
} else {
SerialDebug.print("Error");
}

delay(1000);
}
===============================================================================================
i m using the WioLTE_Cat_NB1_Arduino_Library from Github.
check out the link: https://github.com/lanselambor/WioLTE_C ... no_Library

what if i use hologram sim?? will it solve the problem?? is there any changes required in the source code??

ateeque.rahman1
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri May 17, 2019 5:11 pm

Re: Error: Network initialize timeout in Wio LTE Cat M1/NB-IoT Tracker

Post by ateeque.rahman1 » Mon Jun 03, 2019 3:21 pm

i have tried this code at my Clients Location (i.e.ATLANTA, US) with T-Mobile NB-IOT SIM still the same error takes place.But when i dumped the same code in WIO LTE CAT.NB-IOT(SARA-N410) module with the same SIM, it got successfully registered and we are able to publish the MQTT Packets.
Is there any issue with Wio LTE Cat M1/NB-IoT Tracker??

Post Reply