Hi,
I got my seeeduino stalker v1 with date 12.18.2009 and it seem that the RTC chip DS1307 does not work
I tried to run this program but the time is not running on the serial port output.
[code]/*Reads the value from a Real Time Clock (RTC) DS1307 and displays it in the serial monitor
*
*Created by D. Sjunnesson 1scale1.com d.sjunnesson (at) 1scale1.com
*
*Created with combined information from
*http://www.arduino.cc/cgi-bin/yabb2/YaBB.pl?num=1180908809
*http://www.arduino.cc/cgi-bin/yabb2/YaBB.pl?num=1191209057
*
*
*Big credit to mattt (please contact me for a more correct name…) from the Arduino forum
*which has written the main part of the library which I have modified
*
*/
#include <WProgram.h>
#include <Wire.h>
#include <DS1307.h> // written by mattt on the Arduino forum and modified by D. Sjunnesson
void setup()
{
Serial.begin(9600);
RTC.stop();
RTC.set(DS1307_SEC,1); //set the seconds
RTC.set(DS1307_MIN,23); //set the minutes
RTC.set(DS1307_HR,12); //set the hours
RTC.set(DS1307_DOW,4); //set the day of the week
RTC.set(DS1307_DATE,5); //set the date
RTC.set(DS1307_MTH,3); //set the month
RTC.set(DS1307_YR,9); //set the year
RTC.start();
}
void loop()
{
Serial.print(RTC.get(DS1307_HR,true)); //read the hour and also update all the values by pushing in true
Serial.print(":");
Serial.print(RTC.get(DS1307_MIN,false));//read minutes without update (false)
Serial.print(":");
Serial.print(RTC.get(DS1307_SEC,false));//read seconds
Serial.print(" “); // some space for a more happy life
Serial.print(RTC.get(DS1307_DATE,false));//read date
Serial.print(”/");
Serial.print(RTC.get(DS1307_MTH,false));//read month
Serial.print("/");
Serial.print(RTC.get(DS1307_YR,false)); //read year
Serial.println();
delay(1000);
}
[/code]
I checked already the voltage on the chip where 3,3 V is on the battery pin and 3 V is on the VCC pin. Which seams strange, because it should work with 5 volts. Is it maybe a problem that I power the seeeduino only over USB?
Greetings from Vienna,
Christian