Max. DC Output Current of Seeeduino cards

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
wishkerman
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Aug 09, 2019 11:42 pm

Max. DC Output Current of Seeeduino cards

Post by wishkerman » Sat Aug 10, 2019 3:15 pm

The Seeeduino v4.2 DC Output Current-5V Pin with Micro USB is 500mA and Max with DC Jack Power 2000mA. Therefore, what are the max mA DC output of Seeeduino Lotus V1.1 and Seeeduino Lite?

I wish to connect multiply Groves that require more than 2A Operating Current and I was thinking of using a power supply of 5V with 10A (or more).

Post Reply