usb serial no response

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
john551
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Aug 10, 2018 5:17 am

usb serial no response

Post by john551 » Fri Aug 10, 2018 5:26 am

I'm having a weird time connecting to Seeeduino LoRaWAN board

After connecting USB serial, I send <Enter> and get Command mode response
But thereafter there is no response to any text entered.
I have this on Windows 10 and using a Rasberry Pi.
This behaviour suggestst that the serial connection and driver are correct (?) but that something wrong with data exchange.
I am using Putty on Windows, and minicom on R Pi. CRLF is enabled.


BUT, if I use a serial console on an Android phone using OTG, get the correct response. This is set to CDC driver.
This confirms that the board, cable etc are OK.

Any suggestions what is needed to get either Windows 10 or Raspberry Pi to respond to the serial port?

bill.yu
Elementary-4
Elementary-4
Posts: 420
Joined: Mon Apr 02, 2018 11:05 am

Re: usb serial no response

Post by bill.yu » Fri Aug 10, 2018 9:31 am

Hi, if you want to enter AT command mode, you have to download below code to seeeduino lorawan first. then open the com monitor and config as below.

Code: Select all

void setup()
{
    Serial1.begin(9600);
    SerialUSB.begin(115200);
}

void loop()
{
    while(Serial1.available())
    {
        SerialUSB.write(Serial1.read());
    }
    while(SerialUSB.available())
    {
        Serial1.write(SerialUSB.read());
    }
}
We enter AT+VER, we will see below info.
Image

Bill

Post Reply