DSO V1.1 open source code

Moderators: lily.li, violet, jeremy882, crail.lyu969

FreeZinG

DSO V1.1 open source code

Post by FreeZinG » Mon Nov 23, 2009 10:56 pm

here is the opensource code for DSO Nano.

you can compile and edit it with IAR EWARM .

Modify the APP project that you can make a new UI for DSO , we will follow-up the course of how to make a personalized DSO by yourself.
DS0201_OpenSource.rar
(963.17 KiB) Downloaded 1665 times

elbeem
Pre-kindergarten
Pre-kindergarten
Posts: 31
Joined: Thu Jun 25, 2009 2:59 pm
Location: France

Re: DSO V1.1 open source code

Post by elbeem » Tue Nov 24, 2009 2:26 pm

Thank you, sir

User avatar
slimfish675
Kindergarten
Kindergarten
Posts: 56
Joined: Thu Nov 19, 2009 5:14 pm
Location: Spain

Re: DSO V1.1 open source code

Post by slimfish675 » Tue Nov 24, 2009 9:31 pm

Good move. Thank you

AndreKR
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Nov 25, 2009 7:06 pm

Re: DSO V1.1 open source code

Post by AndreKR » Wed Nov 25, 2009 8:14 pm

Is this older or newer than the "Ver2.01" I had preinstalled on mine?

FreeZinG

Re: DSO V1.1 open source code

Post by FreeZinG » Wed Nov 25, 2009 10:18 pm

It's older than the code that preinstalled ~ but they are much the same

anomalous
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Nov 12, 2009 7:28 am

Re: DSO V1.1 open source code

Post by anomalous » Wed Dec 02, 2009 7:15 am

I have a unit with firmware version 1.1, but people here seem to be talking about a version 2.01 - where would I get his upgrade? I havent found any links on the seed website or this forum for it. also, is there a changelog somewhere?

thanks,

ben

FreeZinG

Re: DSO V1.1 open source code

Post by FreeZinG » Wed Dec 02, 2009 9:11 am

Here is the newest F/W
DS0201_FW_V2.02_SS.rar
(20.01 KiB) Downloaded 2096 times

vhangell
Pre-kindergarten
Pre-kindergarten
Posts: 16
Joined: Thu Dec 17, 2009 5:54 pm

Re: DSO V1.1 open source code

Post by vhangell » Thu Dec 17, 2009 6:10 pm

I tried compiling the codes provided above using IAR 5.40, it requested the workspace to be updated since it was created from an old version of EWARM. After which I was not able to continue with the compilation with the ff. errors:

Linking
Error[Li005]: no definition for "__program_start" [referenced from C:\DS0201_OpenSource\DS0201_DFU\project\EWARM\Debug_FLASH\Obj\
stm32f10x_vector.o]
Error while running Linker

Comparing the provided sourcecode above with the codes provided by bure from the chinese forums, mostly the changes were the logo and the comments (which are very good). I would like to know if the updated source code will be released, since its tagged as an opensource device. Hopefully it will be compatible with the latest IAR IDE (v5.40)

I noticed that the latest f/w shows v1.1 in the logo, I believed the hardware that seeedstudio will release is a 1.3a and not a 1.1.
I also liked the v1.4 f/w from paul (only there was a few spelling errors).

edit:
I fixed the error by adding this code
# define __program_start __iar_program_start

It turns out that, IAR5.xx compilers have considerably changed from IAR4.xx the method for the entry procedure.

FreeZinG

Re: DSO V1.1 open source code

Post by FreeZinG » Fri Dec 18, 2009 9:50 am

this code project is build by IAR 4.20 , the newest F/W is also in IAR 4.20

And the V1.1 in LOGO should be the hardware version , now the newest version is V1.3A , and the F/W version is V2.02.

the F/W of V1.X will be open source and everyone can use it as them wish , but the V2.X F/W will not release the source code , because there is some third party code in it and we don't have the authorization to public it.

and the H/W is all open source for all version.


Thanks
FreeZinG

jbn
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Dec 29, 2009 7:50 pm

Re: DSO V1.1 open source code

Post by jbn » Tue Dec 29, 2009 7:58 pm

I've a question. The firmware can be flashed through DFU FileManager. However is the bootloader protected. I.e can destroy the bootloader by flashing a wrong firmware thus bricking the device. Or can I always reflash the original firmware restoring the device to it's original state?

Post Reply