NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

If you have a new product idea, let us know here!

Moderators: lily.li, violet, jeremy882, lakshanthad, elaine.wu

elaine.wu
Pre-kindergarten
Pre-kindergarten
Posts: 12
Joined: Mon Nov 05, 2018 5:59 pm

NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by elaine.wu » Fri Mar 08, 2019 5:08 pm

NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

The Sipeed MAIX-I module is the first RISC-V 64 AI module based on the powerful KPU K210. As a close partner of Sipeed, we are very excited to announce that we are going to make a Grove HAT for Raspberry Pi based on the Sipeed MAIX-I module, aiming at enabling more possibilities of AI model in areas such as predictive maintenance, anomaly detection, robotics and many more. Grove is a modular plug-and-play ecosystem that includes more than 200 different kinds of sensor, actuators, displays etc.

We are going to release two versions, one based on the Sipeed MAIX-I with WiFi and another without. Both can work as a Raspberry Pi HAT, or work by themselves. The basic function and features are confirmed and listed here. But we are open to suggestions from the community about how to make this product.

Grove AI HAT for Edge Computing without WiFi
Image
Features
Core Module: Sipeed MAIX-1 with WiFi

Peripheral:
1 x LCD Interface
1 x Camera Interface
6 x Grove: 2 x Digital, 1 x I2C, 1 x UART, 2 x Analog
1 x UART Mode Switch

LED:
LED1: Reset
LED2: Boot/User
LED3: Power LED

Power:
1 x USB-C

Others:
Raspberry Pi form factor
12-Bit ADC
USB to UART chip

Grove AI HAT for Edge Computing with WiFi
Image
Features
Core Module: Sipeed MAIX-1 with WiFi

Peripheral:
1 x LCD Interface
1 x Camera Interface
6 x Grove: 2 x Digital, 1 x I2C, 1 x UART, 2 x Analog
1 x UART Mode Switch

LED:
LED1: Reset
LED2: Boot/User
LED3: Power LED

Power:
1 x USB-C

Others:
Raspberry Pi form factor
WiFi Chip ESP8285 inside
12-Bit ADC
USB to UART chip
UPDATE: We just got the first look of this Grove AI HAT for Edge Computing and Raspberry Pi based on the Sipeed MAIX-I, including LCD and Camera Interfaces, connectors for Digital, I2C, UART and Analog.
Image
Image
So, don’t hesitate to share your thoughts and ideas with us in this forum! Check out the first look we have so far and let us know what features you would like to see and have the chance of making it to the final product. If your idea makes it to mass production, of course we will send you a free sample!!!

These products are designed for you and the rest of the community, so it only makes sense for us to listen to what you want for your next AI project.

Subscribe with us now! Don't miss any updates for IoT news and new awesome product releasing!

UPDATE: We are going to release Grove HAT for Edge Computing next week for pre-order!
Finally we take suggestions in this forum by adding 3-Axis Digital Accelerometer, microphone and changing Raspberry Pi 40-Pin connector to SMT style. The USB Type-C port can directly power up Raspberry Pi. Boot Button can be set as user button.
Image
Last edited by elaine.wu on Wed Apr 24, 2019 7:01 pm, edited 5 times in total.

rb9207
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sun Mar 10, 2019 5:35 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by rb9207 » Sun Mar 10, 2019 5:53 pm

I would love to see a SATA interface for either an SSD or a conventional hard drive.

User avatar
lily.li
Staff
Staff
Posts: 30
Joined: Fri Mar 23, 2018 10:23 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by lily.li » Mon Mar 11, 2019 10:13 am

Some inputs from our Facebook community:
屏幕快照 2019-03-11 上午10.11.38.jpg
屏幕快照 2019-03-11 上午10.11.38.jpg (55.07 KiB) Viewed 23822 times

ross728
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Mar 09, 2019 6:14 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by ross728 » Mon Mar 11, 2019 12:40 pm

I reckon that this would make a pretty awesome platform for introducing students to RISC-V, JTAG, and debugging.
Several ideas;

Raspberry Pi as a JTAG tool - please layout the Grove AI HAT PCB to connect the JTAG pins of the SiPEED MAIX-1 to suitable GPIO pins on the HAT connector so that the Raspberry Pi can be used as a JTAG tool. eg https://github.com/synthetos/PiOCD/wiki ... TAG-Dongle

SPI comms with the Raspberry Pi - please layout the Grove AI HAT PCB so that a Raspberry Pi SPI master on the HAT connector (Raspberry Pi is only an SPI master) can talk to an SPI slave on the SiPEED MAIX-1 (SPI much faster than UART...). However, unlike the K210, the Raspberry Pi doesn't have a full FPIOA, so you will have to accommodate its limited choice of HAT pin functions when you layout the Grove AI HAT PCB - only some HAT pins can be used for SPI etc.


Power sharing - please tie the +5Vdc plane on the Grove AI Hat PCB to the +5Vdc pins on the Raspberry Pi HAT connector. Depending on current draw, this will allow both the Raspberry Pi and the HAT to be powered from a single power supply connection (one cable instead of two!)

jeremy882
Staff
Staff
Posts: 45
Joined: Sun Apr 08, 2018 12:40 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by jeremy882 » Tue Mar 12, 2019 12:06 pm

SATA interface is interesting.......however for the basic and medium projects, SD card would be enough with smaller space requirement. If there is needed for SSD, an USB to SATA adapter would be more convenient.

marioalemn
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sat Mar 24, 2018 1:28 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by marioalemn » Fri Mar 15, 2019 12:31 am

A connector for a battery pack would be great! So the battery pack could power both the HAT and the Pi itself.

marioalemn
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sat Mar 24, 2018 1:28 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by marioalemn » Fri Mar 15, 2019 12:38 am

A microphone could be useful.

johnruciak
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Mar 15, 2019 2:22 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by johnruciak » Fri Mar 15, 2019 2:24 am

Make it a real edge device by including LoRaWAN.

bernard.vanhaecke671
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Jun 23, 2018 9:29 am
Location: Mountain View, CA, USA

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by bernard.vanhaecke671 » Fri Mar 15, 2019 2:46 am

Awesome stuff! I suggest to put at least a couple more Grove connector sockets on the board, there seems to be enough room left. This would allow to connect several additional Grove sensors (there are many for about anything), which could be used as additional input to ML models and allow to do sensor fusion projects (because using AI for camera only is somewhat limiting). Grove actuators can be hooked up as well to sockets (relays, motor controller, etc.. there are a lot of Grove accessories) and can for example be controlled from the output of a ML model; this is easy to do. I suggest to put the additional Grove sockets vertically, just like on the Seeeduino Lotus board instead of lining them up at the edge of the PCB. You could probably have 4 analog and 4 digital ports, instead of 2.

yokonav
Pre-kindergarten
Pre-kindergarten
Posts: 18
Joined: Mon Feb 09, 2015 9:10 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by yokonav » Fri Mar 15, 2019 7:16 am

This looks amazing with a lot of possibilities! If we are using it with Raspberry Pi, we do not need wifi, bluetooth, sd card module but of course as a standalone unit we might need it. I was working on the "Recognition of Activities of Daily Lives (ADL)" and there was requirement for a 3-axis accelerometer. The problem is: if we use 3-axis accelerometer grove module, for better result it should be mounted parallel to the board. It would be very helpful to add a 3-axis accelerometer on the board itself which I think would not take much space. It will be beneficial for other use cases like auto-rotate lcd screen, free fall detection (to save data before it crashes!), almost all robotics projects (auto driving) needs it. I am eager to try it out soon!

Post Reply