Issues with Grove Starter Kit for Azure Sphere MT3620 Development Kit (Temp&Humi Sensor(SHT31) I2C signal through MT362

Team,



We are exploring projects on the Azure Sphere MT3620 using MT3620 Grove Shield v1.0 for capturing temperature and Humidity with Grove - Temp&Humi Sensor(SHT31) sensor (I2C) .Now we are facing a error while setting up the project could you please check the below and help us to fix it .





Steps Followed :

  1. Connections

    • Connect Grove - Temp&Humi Sensor(SHT31) to I2C port of MT3620 Grove Shield.

    • Plug the MT3620 base shield to Azure Sphere MT3620 Development board.

    • Plug the USB cable to Azure Sphere MT3620 Development board and PC.
  2. Software

    • Downloaded the source code and made all the changes as per informed in the page (<LINK_TEXT text=“http://wiki.seeedstudio.com/Grove_Start … pment_Kit/”>http://wiki.seeedstudio.com/Grove_Starter_Kit_for_Azure_Sphere_MT3620_Development_Kit/</LINK_TEXT> )



    Issue Occurred:



    A. When Remote GDB Debugger option is hit we can see the project did not produce the temperature and humidity result in the device output .





    Troubleshoot Steps:



    A. We tried to debug the code by adding checkpoint and found there was infinite loop in the below code

    while (i2cState != I2C_OK)

    {

    SC18IM700_ReadReg(fd, 0x0A, &i2cState);

    }







    B. We tried to check the value of I2C_OK and received the below error .







    C. When we checked the output it stalls after this .







    Help Needed :

    Could you please work with us or let us know if there are any troubleshoot or solutions applicable for the same . We are happy to work on a remote session to fix this issue .





    Note : Azure sphere Kit has been configured as per the page <LINK_TEXT text=“https://docs.microsoft.com/en-us/azure- … l/overview”>https://docs.microsoft.com/en-us/azure-sphere/install/overview</LINK_TEXT>



    Hardware Connection



    Base Azure Sphere MT3620

    Shield MT3620 Grove Shield v1.0

    Sensor Grove - Temp&Humi Sensor(SHT31)





    GitHub Source Code :

    https://github.com/Seeed-Studio/MT3620_Grove_Shield





    We are looking forward for a solution from you .



    Thanks

    Jay
    C_QUERY.png
    C_QUERY_IMMEDIATEWINDOW.png
    C_OUTPUTFILES.png

Any suggestion/solution on the above is much appreciated