Board not connected to Virtualbox windows 10 guest vm

Welcome to ask questions or discuss anything related to Azure Sphere products

Moderators: lily.li, violet, seth.welday

Post Reply
kursatgol
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Wed Oct 24, 2018 4:29 pm

Board not connected to Virtualbox windows 10 guest vm

Post by kursatgol » Tue Nov 20, 2018 12:48 am

Hi All,

I planned to use a vm for MT3620 development and installed windows 10 to my virtualbox with 50 GB storage and 8 GB memory but i could not connect the board to my vm succesfully. Could you please advice me about this issue? Here enclosed a screenshot from my device manager.
board_not_connected_on_vm.png
board_not_connected_on_vm.png (22.79 KiB) Viewed 1931 times
regards.

kursat

kursatgol
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Wed Oct 24, 2018 4:29 pm

Re: Board not connected to Virtualbox windows 10 guest vm

Post by kursatgol » Thu Nov 22, 2018 10:29 pm

Hi All,

I am answering my self question. After a long investigation from the net i found below steps and now its working properly.

Step 1) Download and install the exact extension pack from internet for virtualbox to recognize the usb2.0 protocol. Because Azure Sphere devkit is running on usb2.0. Here is the web-site for download.
https://download.virtualbox.org/virtual ... ox-extpack
Step 2) Install the extension pack as next-next-next steps.
vbox_ext_pack_01.png
vbox_ext_pack_01.png (24.66 KiB) Viewed 1927 times
Step 3) Set the vm usb settings like below and boot the vm from virtualbox. After boot process wait near 2 minutes for self-installation of board drivers. Do nothing while it is installing the 3 com port drivers. Here is the below proper settings for vm.
usb_settings_for_vm.png
usb_settings_for_vm.png (62.97 KiB) Viewed 1927 times
regards. enjoy with your installed board.

kursat

bill.yu
Junior-6
Junior-6
Posts: 691
Joined: Mon Apr 02, 2018 11:05 am

Re: Board not connected to Virtualbox windows 10 guest vm

Post by bill.yu » Wed Nov 28, 2018 3:33 pm

Hi kursat

thanks for the sharing on the azure sphere development board development on VM.

best rgds
Bill

User avatar
andre.ml.curvello
Pre-kindergarten
Pre-kindergarten
Posts: 14
Joined: Thu May 10, 2018 7:19 pm
Contact:

Re: Board not connected to Virtualbox windows 10 guest vm

Post by andre.ml.curvello » Sun Dec 16, 2018 6:39 pm

Hi @kursatgol, how are you?

Thanks for sharing this!
This has bring up another doubt other users may have:
- You are using a VM on a Windows Host systems. But... If you are using on a Linux Host system?
I'll try that when I have the opportunity.

This is necessary, as to develop for Azure Sphere Kit is only possible, for now, with Visual Studio IDE (on Windows).
Linux users will have to do this workaround with VM.

Best,
Andre.

Post Reply