DepthEye3D issues on mac (H1AsciiSample)

Please post any suggestions or complaints that you have for Seeed, Seeed products and services, and we'll make it better for you.

Moderators: lily.li, violet

Post Reply
edgrjr
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Nov 21, 2018 3:21 am

DepthEye3D issues on mac (H1AsciiSample)

Post by edgrjr » Sat Nov 24, 2018 1:40 pm

Hello All,

I am unable to load the SDK Ascii Sample from the github instructions
Link: https://github.com/pointcloud-ai/DepthEyeSdk

I get the following warning when making the file

MacBook-Pro:build estre$ make
Scanning dependencies of target deptheye
[ 25%] Building CXX object src/CMakeFiles/deptheye.dir/DepthEyeInterface.cpp.o
[ 50%] Linking CXX static library ../lib/libdeptheye.a
[ 50%] Built target deptheye
Scanning dependencies of target H1AsciiSample
[ 75%] Building CXX object test/CMakeFiles/H1AsciiSample.dir/H1AsciiSample.cpp.o
[100%] Linking CXX executable ../bin/H1AsciiSample
ld: warning: directory not found for option '-L/Users/xx/Downloads/DepthEyeSdk-master/./lib'
[100%] Built target H1AsciiSample

Then if I run H1AsciiSample I get:
MacBook-Pro:build estre$ ./bin/H1AsciiSample
dyld: Library not loaded: @rpath/libusb-1.0.0.dylib
Referenced from: /Users/xx/Downloads/DepthEyeSdk-master/./third_party/voxelsdk_osx/lib/libvoxel.34.dylib
Reason: image not found
Abort trap: 6


Can anyone at least point me with a point of start? I tried looking into the ld warning but I can't find anything useful. Any help would be appreciated!

bill.yu
Elementary-5
Elementary-5
Posts: 597
Joined: Mon Apr 02, 2018 11:05 am

Re: DepthEye3D issues on mac (H1AsciiSample)

Post by bill.yu » Mon Nov 26, 2018 2:15 pm

Hi there,
Because the computer is missing the libusb library, please follow the http://macappstore.org/libusb/ guide to install the libusb library to solve the problem. thanks.

Post Reply