Page 1 of 1

problems with uploading programs to seeeduino

Posted: Sat Oct 27, 2018 10:45 pm
by augustq
Hi,

I am playing with the seeeduino LoraWAN wGPS-board. I have problems uploading a program to the board.

My environment:
PC: Ubuntu 18.04
Software: Arduino Ide 1.8.5
seeeduino: 06/07/18

Compiling a program within the Ide works, uploading the code to the board stops. Different messages appear, one of them is:

Code: Select all

No device found on ttyACM0
Set binary mode
Beim Hochladen des Sketches ist ein Fehler aufgetreten
Send auto-baud
Set binary mode
The board is connected to the PC via USB, Ubuntu creates it as /dev/ttyACM0. Via the ls-command I can check this, dmesg also reports this:

Code: Select all

[ 7693.740790] usb 1-4: new full-speed USB device number 20 using xhci_hcd
[ 7694.056674] usb 1-4: New USB device found, idVendor=2886, idProduct=000c
[ 7694.056678] usb 1-4: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 7694.059463] cdc_acm 1-4:1.0: ttyACM0: USB ACM device

Code: Select all

august@August-Ryzen:~$ ls -l /dev/ttyA*
crw-rw---- 1 root dialout 166, 0 Okt 26 11:07 /dev/ttyACM0
august@August-Ryzen:~$
Can you pleas give me an advice.
Thenkas
AugustQ

Re: problems with uploading programs to seeeduino

Posted: Fri Nov 23, 2018 10:16 am
by bill.yu
Hi there,

please double click the reset button and see if the issue is solved. thanks.