Recommendation for a vibration motor working with [Seeed XIAO nRF52840 Sense.]

I don’t see the charging circuit of the LiPo battery on the schematic.

If you plan to use the battery charging chip of the Xiao nRF52840, you can’t use a switch to disconnect the battery.

As most embedded systems operate, the whole circuit is always on but the nRF52840 enters deep sleep. Use a temporary push button connected to an interrupt-capable GPIO as trigger to wake it up.

1 Like