Hi PJ - Another problem I’m having with my XIAO ESP32S3 board is that it frequently gets stuck during the code flash stage. The error message I get is as follows:
Sketch uses 238501 bytes (7%) of program storage space. Maximum is 3342336 bytes.
Global variables use 18188 bytes (5%) of dynamic memory, leaving 309492 bytes for local variables. Maximum is 327680 bytes.
esptool.py v4.5.1
Serial port /dev/ttyACM0
Connecting…
Chip is ESP32-S3 (revision v0.2)
Features: WiFi, BLE
Crystal is 40MHz
MAC: 98:3d:ae:ed:07:e4
Uploading stub…
Running stub…
Stub running…
Changing baud rate to 921600
A fatal error occurred: No serial data received.
Failed uploading: uploading error: exit status 2
Also, the red LED next to the Reset button sometimes turns on and stays on for a long time. That said, at the moment, the red LED is NOT on and I’m still getting the above error message. - Thanks - Jim