Hi there!
@Pecako2001
Please watch the thread from Nvidia forum.
If you want mainly to work ZED X with J4012 it can be done, but not all the functionality of the J4012 will be there.
I can make the stream from ZED X now, to play with some python examples.
I have stopped for the moment to tune the solution. For what I need now is almost ok.
The solution in my case was to use the Nvidia SDK (is not what SEEED says on their wiki) and to install Jetpack 6.0. Then I have installed from Stereolabs drivers 1.1.1, not for the capture card , but for the Orin device that STEREOLABS have (https://stereolabs.sfo2.cdn.digitaloceanspaces.com/utils/drivers/ZEDX/1.2.0/R36.3/stereolabs-zedbox-onx16_1.2.0-LI-MAX96712-all-ZEDBOX-L4T36.3.0_arm64.deb)
I have seen now, that STEREOLABS have now a new driver 1.2.0 (I have not tested yet).
For short:
- if you have time and little money buy J4012 from SEED + ZEDX and capture card from Stereolabs (maybe the new driver from Stereolabs helps, but I have to test it…
- if you have less time buy all from Stereolabs.
In my case it was a problem because Stereolabs does not let you open the Orin BOX.
@liaifat85 Can you point to a solution. I have tested a lot of config file with no luck for the moment.