Search found 85 matches

by bestlux
Thu Apr 11, 2019 3:02 pm
Forum: General Info - Guidance
Topic: Can-usb analyzer
Replies: 1
Views: 1323

Re: Can-usb analyzer

Hello,
could you pls specify your problem? I can not read without punctuation. How can I help you?
I am sorry for now know more about this app too, maybe you can contact their technical support.
by bestlux
Wed Apr 10, 2019 1:49 pm
Forum: Grove
Topic: using Grove - BLE to detect iBeacons
Replies: 1
Views: 2079

Re: using Grove - BLE to detect iBeacons

Hello,
Here is official documentation of iBeacon of HM13 module, I hope it can help.
http://www.huamaosoft.com/iBeacon_en.zip
by bestlux
Tue Apr 09, 2019 4:02 pm
Forum: Wio Series
Topic: Download firmware to Wio LTE CAT M1/NB-IoT?
Replies: 1
Views: 818

Re: Download firmware to Wio LTE CAT M1/NB-IoT?

Hello,
Pls have a look at the seeed wiki for the firmware and tutorial.
Thx!
Links: http://wiki.seeedstudio.com/Wio_LTE_Cat ... T_Tracker/
by bestlux
Tue Apr 09, 2019 3:09 pm
Forum: Shields
Topic: Wifly v2.0 static ip problem
Replies: 2
Views: 1219

Re: Wifly v2.0 static ip problem

Hello,
I do not know what your wifi sharing method so I can not give you more advice, sometimes it is not shown in the hotspot software in dhcp mode.
by bestlux
Tue Apr 09, 2019 2:09 pm
Forum: Arduino & Seeeduino
Topic: How to send gps data without USB cable connected from seeeduino lorawan to Loriot server
Replies: 4
Views: 1458

Re: How to send gps data without USB cable connected from seeeduino lorawan to Loriot server

Hello,
Pls tell me how did you supply the power(a pic of wire connection is primary) and what kind of battery did you use.
Thx!
by bestlux
Tue Apr 09, 2019 10:11 am
Forum: Grove
Topic: VOC and eCO2 gas sensor (SGP30) doubts
Replies: 7
Views: 913

Re: VOC and eCO2 gas sensor (SGP30) doubts

Hello, The function store_baseline() stored the baseline in the EEPROM, if you comment it, this example is just the same as a normal reading example. You should go into the function and see which step does it stuck. void store_baseline(void) { static u32 i=0; u32 j=0; u32 iaq_baseline=0; u8 value_ar...
by bestlux
Tue Apr 09, 2019 9:37 am
Forum: Grove
Topic: JST connector on grove sunlight sensor
Replies: 1
Views: 417

Re: JST connector on grove sunlight sensor

Hello,
It is feasible in principle. But you'd better use absorb gun with a welding torch to do it. There is also a high possibility of damage lol.
by bestlux
Tue Apr 09, 2019 9:24 am
Forum: Wio Series
Topic: Wio LTE Cat.NB-IoT 7/16/2018 Works while 5/26/2018 fails
Replies: 1
Views: 802

Re: Wio LTE Cat.NB-IoT 7/16/2018 Works while 5/26/2018 fails

Hello,
There might be some problem with your firmware if nothing wrong with your hardware, so you can try burning the firmware[/url][/url] yourself.
Thanks!

Links: http://wiki.seeedstudio.com/Wio_LTE_Cat ... e-firmware
by bestlux
Tue Apr 02, 2019 9:49 am
Forum: Arduino & Seeeduino
Topic: rtl8710 wifi module eagle library needed
Replies: 1
Views: 711

Re: rtl8710 wifi module eagle library needed

Hello,
The module is controlled by AT command, that means you just need to use serial port or create a software serial port to control it, and those libraries are in Arduino ide naturally.
Thx
by bestlux
Tue Apr 02, 2019 9:40 am
Forum: Grove
Topic: VOC and eCO2 gas sensor (SGP30) doubts
Replies: 7
Views: 913

Re: VOC and eCO2 gas sensor (SGP30) doubts

Hello, The "Serial start" is in line 101 of the function setup() in baseline_operation_example.ino. and then it should output"get ram signal!" or "error reading signals" I'm afraid there is something wrong. I guess it is with the following lines of code. So could you tell me which Arduino board are ...