Search found 85 matches

by motopasscode
Sat May 14, 2016 2:10 pm
Forum: DSO
Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
Replies: 84
Views: 123533

Re: BenF 3.x FW on new LCD driver devices [flick. screen sol

bazbroom, I don't know what your needs are so take what I say with grain of salt. I know of 6 different versions DS201 in 3 physical forms on the market. Pictures here http://www.seeedstudio.com/wiki/DSO_Nano These I know, maybe there are others... Version 1. DS201/DSO Nano v1 Version 2. DS201/DSO ...
by motopasscode
Sat May 07, 2016 2:50 am
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 530308

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

I could not run QUSDCFG.EXE on Windows 7 64bit. C:\>QUADCFG.EXE This version of C:\QUADCFG.EXE is not compatible with the version of Windows you're running. Check your computer's system information to see whether you need a x86 (32-bit) or x64 (64-bit) version of the program, and then contact the so...
by motopasscode
Tue May 03, 2016 2:44 am
Forum: DSO
Topic: DSO201 firmware query newbie
Replies: 3
Views: 3671

Re: DSO201 firmware query newbie

Great,

One thing I will mention is if the DSO has onboard 2M flash then BenF firmware features related to SD card such as Save BMP/Load Buff will not work.

It seems it would possible to patch in new functions but I don't have access to DSO with onboard flash to try.
by motopasscode
Sun May 01, 2016 5:02 am
Forum: DSO
Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
Replies: 84
Views: 123533

Re: BenF 3.x FW on new LCD driver devices [flick. screen sol

Just received the Nano V3 and I tried installing BenF 3.64 and it failed. I accidentally deleted the firmware V3.45D that came with the Nano V3. Is their a site where I can either get the BenF app and lib hex files that will work the scope, or at least get the V3.45D app and lib that came with it? ...
by motopasscode
Sun May 01, 2016 4:29 am
Forum: DSO
Topic: DSO201 firmware query newbie
Replies: 3
Views: 3671

Re: DSO201 firmware query newbie

Hi, Have a read here and provide hardware details about your device. Have you tried v4.30? The issue you describe could be DFU compatibility issue or device license. I recommend you try Benf 3.64 V3 firmware which works on new DFU V3.45D. The patch was done by rimidalv007 here and I fixed minor hex ...
by motopasscode
Sat Apr 30, 2016 3:39 pm
Forum: DSO
Topic: Unable to update with DFU v3.11C
Replies: 5
Views: 3718

Re: Unable to update with DFU v3.11C

Well, you're not alone. I had a similar mishap recently when I upgraded with a version of Wildcat for 2.81. I had the marco-sinnati firmware. Sys and App. Loaded that and all was well. The new 2.81 firmware might be overwriting the sys in some part. I recovered the working of my DSO but the SEEED l...
by motopasscode
Sat Apr 30, 2016 2:37 pm
Forum: DSO
Topic: DSO201 V4.30 Firmware port for Hw V1/V2 lcd 7781 LCD
Replies: 0
Views: 2644

DSO201 V4.30 Firmware port for Hw V1/V2 lcd 7781 LCD

WARNING : For some reason I had to reformat SD card with Allocation unit size 8192. When I switched to BenF, I must reformat SD card with SDFormatter program because of SD error message. Make sure you backup! I was curious about official minidso DS201 V4.30. I could not find a .dfu build for old Hw...
by motopasscode
Wed Apr 20, 2016 8:48 am
Forum: DSO
Topic: New DFU V3.45
Replies: 5
Views: 6017

Re: New DFU V3.45

@motopasscode - That was exactly it! Revising the start segment was the key. Now THIS is the DSO I thought I was buying. Thank you for the assistance. Awesome! If possible, do you think you could edit your original post to mention Benf 3.64 on DFU 3.45D and attach the fixed hex. I think it would he...
by motopasscode
Sun Apr 17, 2016 3:04 pm
Forum: DSO
Topic: New DFU V3.45
Replies: 5
Views: 6017

Re: New DFU V3.45

The new bootloader might not be happy with bogus "05 - Start Linear Address Record" found at the end of the hex file on line, :0400000500000000F7 Try replace it with :040000050800C1210D You can also try to remove it completely. Other thing I see in 4.30 is that they joined LIB and APP and the is no ...
by motopasscode
Tue Apr 12, 2016 10:39 am
Forum: DSO
Topic: DSO Nano Electron 007 Firmware for V1/V2 7781 LCD
Replies: 1
Views: 1716

Re: DSO Nano Electron 007 Firmware for V1/V2 7781 LCD

screenshot.png
A version with 2 Letters popup menu, my favorite :geek: