Search found 34 matches

by Tobe
Sat May 19, 2012 2:56 pm
Forum: To Be Classified
Topic: Keyboard plus antenna
Replies: 1
Views: 1986

Re: Keyboard plus antenna

Hi,
That is so cool~
We will think about it,and try to develop that.
Thank You!
by Tobe
Sat May 19, 2012 2:47 pm
Forum: Bee series & WSN
Topic: Bluetooth Bee Standalone & DFROBOT IO Expansion Shield
Replies: 6
Views: 5226

Re: Bluetooth Bee Standalone & DFROBOT IO Expansion Shield

For the Bluetooth Bee standalone,it already have a MCU there,so you can download the demo code directly to the Bluetooth bee. For you code,there have a problem,for the D0,D1 is the hardware Serial port,so for you code,you use the software and the hardware serial port as the same one,so it's confuse ...
by Tobe
Tue May 15, 2012 3:55 pm
Forum: Arduino & Seeeduino
Topic: rainbowduino V2 not working
Replies: 4
Views: 2007

Re: rainbowduino V2 not working

First,i think you should upload the firmware(you can download from here: http://code.google.com/p/neorainbowduino/downloads/detail?name=neorainbow-0.82.zip&can=2&q= ) to the rainbowduino,as the wiki said,use the arduino to connect the rainbowduino like this, http://www.seeedstudio.com/wiki/images/8/...
by Tobe
Tue May 15, 2012 3:34 pm
Forum: Shields
Topic: Mifare Ultralight C with NFC Shield V1.0
Replies: 5
Views: 4389

Re: Mifare Ultralight C with NFC Shield V1.0

Ok!
Thank you too.
by Tobe
Tue May 15, 2012 2:52 pm
Forum: Shields
Topic: Mifare Ultralight C with NFC Shield V1.0
Replies: 5
Views: 4389

Re: Mifare Ultralight C with NFC Shield V1.0

Hi, For this card [ http://www.seeedstudio.com/depot/1356mhz-rfid-book-tag-p-1067.html?cPath=144_153 ],is just for read the card number,it can not read or write the memoryblocks. If you wan to Read&write the card,you can buy this: http://www.seeedstudio.com/depot/mifareone-rfid-card-1356mhz-p-240.ht...
by Tobe
Tue May 15, 2012 2:30 pm
Forum: Fusion PCB/ PCBA Services
Topic: High speed wifi module
Replies: 1
Views: 1527

Re: High speed wifi module

Hi there:
I'm sorry to tell you that now we don't have that wifi module and the ADC converter,but if we find something that is fit to your project,we will let you know.
by Tobe
Tue May 15, 2012 11:44 am
Forum: Arduino & Seeeduino
Topic: seeeduino film battery meter
Replies: 1
Views: 1264

Re: seeeduino film battery meter

I'm so sorry for that we have no think about that thing,so the seeeduino film there is no way to know the voltage of the battery.
by Tobe
Mon May 14, 2012 6:08 pm
Forum: Shields
Topic: Mifare Ultralight C with NFC Shield V1.0
Replies: 5
Views: 4389

Re: Mifare Ultralight C with NFC Shield V1.0

I try the code you are posting,It can work succeed.So your code is OK.
I think is the Card problem or you can try to put the card on the NFC shield for a little long time.(do not take it away so quick)
by Tobe
Mon May 14, 2012 6:03 pm
Forum: Arduino & Seeeduino
Topic: Uploading firmware to Rainbowduino v3.0
Replies: 4
Views: 2081

Re: Uploading firmware to Rainbowduino v3.0

Hi~ sorry to confuse u,
what i mean is before you are upload the code to the rainbowduino,you can try to pressing the reset button on the reainbowduino,and then upload the code.
by Tobe
Mon May 14, 2012 4:01 pm
Forum: Arduino & Seeeduino
Topic: rainbowduino V2 not working
Replies: 4
Views: 2007

Re: rainbowduino V2 not working