Search found 34 matches

by Tobe
Fri May 25, 2012 1:49 pm
Forum: Bee series & WSN
Topic: bluetooth working. why ?
Replies: 6
Views: 3726

Re: bluetooth working. why ?

Hi,there Thanks for your feedback,for the xbee shield while is connect to the D11,D12,that is compatible for the mega,the mega message: Not all pins on the Mega and Mega 2560 support change interrupts, so only the following can be used for RX: 10, 11, 12, 13, 50, 51, 52, 53, 62, 63, 64, 65, 66, 67, ...
by Tobe
Fri May 25, 2012 1:17 pm
Forum: Bee series & WSN
Topic: Bluetooth BEE : Connect:failed
Replies: 4
Views: 3319

Re: Bluetooth BEE : Connect:failed

Hi,there
If you want to connect to the device,you have to know its address and name.
You can consult the demo code of the master.
by Tobe
Fri May 25, 2012 11:26 am
Forum: Bee series & WSN
Topic: Bluetooth Bee Standalone & DFROBOT IO Expansion Shield
Replies: 6
Views: 5298

Re: Bluetooth Bee Standalone & DFROBOT IO Expansion Shield

Hi,
I try the mega,but it can not work.
Try the UNO,It's ok.
I just follow the linkhttp://arduino.cc/en/Tutorial/ArduinoISP
by Tobe
Fri May 25, 2012 9:25 am
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8221

Re: Arduino Uno + BluetoothShield (SLD63030P)

Hi,
Can you take a picture for me,so i can see the hardware and check if it is right.
by Tobe
Thu May 24, 2012 5:18 pm
Forum: Grove
Topic: HMC5883
Replies: 11
Views: 6320

Re: HMC5883

The 0x3D 0x06 just for the arduino firmware,that mean is to read 6 datas from the HMC5883.
For the code,you can consult the arduino demo code.
by Tobe
Thu May 24, 2012 4:36 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8221

Re: Arduino Uno + BluetoothShield (SLD63030P)

Hi,there As you said,you use the Mega2560 Board,for that,we upload the new Firmware of the Bluetoothshield,you can download it from: http://www.seeedstudio.com/wiki/Bluetooth_Shield There have the code for mega using the hardware serial or software serial,so depanding on the hardware to choice the d...
by Tobe
Tue May 22, 2012 5:42 pm
Forum: Arduino & Seeeduino
Topic: Rainbowduino V3.0b Newbie
Replies: 12
Views: 6588

Re: Rainbowduino V3.0b Newbie

Hi there,
For the USB Driver,
if you can,you can try this commend to your linux:"lsusb" before you plug in the usb cable and after you plug in the usb cable.
catch the picture and post to here.
Thank you.
by Tobe
Tue May 22, 2012 4:38 pm
Forum: Shields
Topic: Music Shield not playing
Replies: 29
Views: 30550

Re: Music Shield not playing

Hi there: I fllow the wiki,try the Demo 1,for the Demo 1,there has some notic,when you are download the Music v1.2.zip and uncompress it under the arduino-1.0 lib floder, then do not download the Demo 2 's lib,just say Music v1.2 and MusicShieldNewSDLib can not be in the same Lib floder. After that,...
by Tobe
Tue May 22, 2012 4:07 pm
Forum: Grove
Topic: HMC5883
Replies: 11
Views: 6320

Re: HMC5883

If you can,you can post your i2cRead_Address function how to achieve,also the i2cWrite_Data function. here is the change of the code: //must read all six registers plus one to move the pointer back to 0x03 i2cSendStart(); i2cWaitForComplete(); i2cRead_Address(0x3D); //read from HMC i2cWaitForComplet...