Search found 34 matches

by Tobe
Wed Jun 20, 2012 4:59 pm
Forum: Arduino & Seeeduino
Topic: Noise on Arduino PWM pins?
Replies: 3
Views: 2629

Re: Noise on Arduino PWM pins?

Try to use the external power on the GPRS shield too.the usb just power the Arduino Uno.
by Tobe
Wed Jun 20, 2012 4:37 pm
Forum: To Be Classified
Topic: Weird things happening with LED matrix
Replies: 1
Views: 1893

Re: Weird things happening with LED matrix

Hi Joshie, What I think is your array of the "abcd...." is code is use char,it is use the ram,so it is waste the ram, so what i suggest is change this char* a[8]={ "00111100", "01111110", "01100110", "01100110", "01111110", "01111110", "01100110", "01100110"}; into to this: const char* a[8]={ "00111...
by Tobe
Wed Jun 20, 2012 4:25 pm
Forum: Shields
Topic: Music Shield - stopFile Function
Replies: 2
Views: 2527

Re: Music Shield - stopFile Function

Hi dincay,
Here is the new library of the music shield,It can contral the music by software now,there has the readme file,if you don't how to use it,you can read that.
http://seeedstudio.com/wiki/File:Librar ... 120619.zip
by Tobe
Mon Jun 04, 2012 5:27 pm
Forum: Shields
Topic: Bluetooth shield instalation problem
Replies: 2
Views: 1947

Re: Bluetooth shield instalation problem

Hi there,
You are using the Arduino IDE 1.0,so you need to he download "Bluetooth Shield Demo Code for Arduino 1.0" on the wiki.
The Code Link:http://www.seeedstudio.com/wiki/images/ ... ino1.0.zip
by Tobe
Mon Jun 04, 2012 5:21 pm
Forum: To Be Classified
Topic: Can i upload program to Film using Bluetooth film module?
Replies: 1
Views: 1766

Re: Can i upload program to Film using Bluetooth film module

Hi there,
Bluetooth can not upload program to Film.
by Tobe
Fri Jun 01, 2012 4:07 pm
Forum: Shields
Topic: gprs and sms read
Replies: 1
Views: 1703

Re: gprs and sms read

You can try

Code: Select all

AT+CMGF=1
AT+CMGL="all"
This can read all the message

Code: Select all

AT+CMGF=1
AT+CMGL="rec unread"
This will read unread message
by Tobe
Thu May 31, 2012 4:43 pm
Forum: Shields
Topic: GPRS Shield - How to answer an incomming call or SMS?
Replies: 1
Views: 1669

Re: GPRS Shield - How to answer an incomming call or SMS?

For the Calling income number,you can set "AT+CLIP=1" then it will show the income call number. you can search the AT command in the datasheet by find "CLIP". For the SMS,you can use the AT+CMGR,you also can check it into the datasheet. SIM900ATCommand: http://garden.seeedstudio.com/images/a/a0/SIM9...
by Tobe
Wed May 30, 2012 5:02 pm
Forum: Arduino & Seeeduino
Topic: Daisy-chaining RGB LED matrices using Rainbowduino V3.0b
Replies: 3
Views: 2556

Re: Daisy-chaining RGB LED matrices using Rainbowduino V3.0b

Hi,Tim The Rainbowduino V3.0 is not compatible to Rainbowduino V2.0,So the firmware is also not compatible. For now,the firmware of the rainbowduino is not updata anymore.What is using in rainbowduino V2.0 is : http://code.google.com/p/neorainbowduino/ So,for now,we don't have a new firmware for the...
by Tobe
Tue May 29, 2012 4:52 pm
Forum: Arduino & Seeeduino
Topic: how to command rainbowduino v2?
Replies: 1
Views: 1674

Re: how to command rainbowduino v2?

Hi,there Sorry for the inconvenience brought. For this problem,I try it on my raindowduino V2.0,and it can work great. I just follow this to finish: 1.Download all the thing we need in here: http://code.google.com/p/neorainbowduino/downloads/detail?name=neorainbow-0.82.zip&can=2&q= Uncompress the zi...
by Tobe
Tue May 29, 2012 2:28 pm
Forum: Shields
Topic: Music Shield Stopping Recording
Replies: 1
Views: 1707

Re: Music Shield Stopping Recording

Hi,there
Sorry for the inconvenience brought.
Our engineer is working on the new firmware.
After he finish that,We will upload it to the WIKI.