Search found 14 matches

by vernarim
Thu Apr 21, 2011 12:46 pm
Forum: DSO
Topic: DSO Quad bandwidth
Replies: 117
Views: 131729

Re: DSO Quad bandwidth

Channels A & B can simultaneously display 3.546Mhz square waves (which is 10% of the Max sample rate of 36MS/s) with reasonable shape. I have tested that just yesterday using an HP signal generator, a LeCroy scope an the DSO Quad. I must confirm that a 5Vpp square wave is altered as low as 1 MHz. A...
by vernarim
Tue Apr 19, 2011 2:45 am
Forum: DSO
Topic: DSO features checkup
Replies: 4
Views: 5346

Re: DSO features checkup

I do not think the analog bandwidth is said to be 72 MHz. The sample rate is 72 Mega samples / s though. I have the same suspect, but the product description clearly states: DSO Quad is a pocket size 4 channel digital oscilloscope for common electronic engineering tasks. It's based on ARM cortex M3...
by vernarim
Mon Apr 18, 2011 8:19 pm
Forum: DSO
Topic: DSO features checkup
Replies: 4
Views: 5346

DSO features checkup

Hi there. Just today I have managed a small checkup of my brand-new DSO Quad, testing it with some signals and a pro scope. Well, I have connected a HP signal generator 0 dbm (sine wave approx 0.5Vpp) on a 50 Ohms load, together with the Quad (ch-A) and a LeCroy scope (5GHz bandwidth). So far so wel...
by vernarim
Fri Apr 15, 2011 1:09 am
Forum: DSO
Topic: PC interface planned?
Replies: 3
Views: 2865

PC interface planned?

Hi there! I have received the DSO Quad two days ago and I have enjoyed it very much. I'd like to ask you some questions... The knobs aren't practical: they are too small and I have difficulty to press them. Over that, to scan the various functions, you have to shift the knob left or right. Now, why ...