Search found 735 matches

by bill.yu
Fri Aug 03, 2018 9:11 am
Forum: ReSpeaker
Topic: Audio Output Quality is 16 KHz on v2
Replies: 13
Views: 5236

Re: Audio Output Quality is 16 KHz on v2

Hi there, I talked with the software engineer and the 16Khz is related with algorithm. Current we do not have plan to update the algorithm. thanks for understanding.

Bill
by bill.yu
Fri Aug 03, 2018 9:10 am
Forum: ReSpeaker
Topic: AEC
Replies: 6
Views: 2147

Re: AEC

Hi, I talked with the software engineer and the 16Khz is related with algorithm. Current we do not have plan to update the algorithm. thanks for understanding.

Bill
by bill.yu
Thu Aug 02, 2018 9:46 am
Forum: Shields
Topic: CAN-BUS Shield v1.2 novice help needed
Replies: 4
Views: 1570

Re: CAN-BUS Shield v1.2 novice help needed

Hi Mark,

Thanks for sharing the story. Do you mind posting the youtube in the forum in future? So other people can learn from it. thanks.

Bill
by bill.yu
Thu Aug 02, 2018 9:43 am
Forum: Arduino & Seeeduino
Topic: Ways to erase flash with Serial1 conflict on Cloud?
Replies: 7
Views: 2627

Re: Ways to erase flash with Serial1 conflict on Cloud?

Hi there, please try follow below instructions. thanks. 1. Plug in the USBtiny to PC USB port 2. Power the arduino yun through USB 3. Plug the 6 pin cable from the USBtinyISP into the Arduino yun 4. Start up Arduino IDE 5. Select the Arduino Yun in the Tools->Board menu 6. Do not select a COM/Serial...
by bill.yu
Thu Aug 02, 2018 9:08 am
Forum: Complaints and Suggestions
Topic: when connected to hdmi port of laptop with win 10 display not working
Replies: 2
Views: 3300

Re: when connected to hdmi port of laptop with win 10 display not working

Hi there, please take a picture of your setup. thanks.

Bill
by bill.yu
Wed Aug 01, 2018 9:46 am
Forum: ReSpeaker
Topic: problem connecting terminal via OTG
Replies: 3
Views: 1179

Re: problem connecting terminal via OTG

Hi there, do you have the usb to ttl adapter? if yes, please follow below instructions and provide the screen info. thanks. B. Connection via The UART port In this section we will guide you how to establish a connection from your computer to your ReSpeaker using your USB to TTL adapter which will be...
by bill.yu
Wed Aug 01, 2018 9:42 am
Forum: Raspberry Pi
Topic: Error using Moisture Sensor v1.4
Replies: 3
Views: 3108

Re: Error using Moisture Sensor v1.4

Hi, please try update the firmware and see if the issue is solved. thanks.

https://www.dexterindustries.com/GroveP ... -firmware/

Bill
by bill.yu
Wed Aug 01, 2018 9:35 am
Forum: Arduino & Seeeduino
Topic: Arduino Servo control problem, external servo power source
Replies: 0
Views: 892

Re: Arduino Servo control problem, external servo power source

Hi there, please take a picture about the whole setup. we can see if we can simulate the issue. thanks.
Bill
by bill.yu
Wed Aug 01, 2018 9:33 am
Forum: Arduino & Seeeduino
Topic: LoRaWan Library source code
Replies: 4
Views: 2081

Re: LoRaWan Library source code

Hi Jimgi, please try one more time by following below instructions. 1. add seeeduino lorawan into board manager by following http://wiki.seeedstudio.com/Seeed_Arduino_Boards/ 2. open arduino ide--> file-->preferences-->settings-->more preferences can be edited directly in the file 3. then click the ...
by bill.yu
Wed Aug 01, 2018 9:26 am
Forum: Wio Series
Topic: Problem connecting to Private APN
Replies: 3
Views: 2359

Re: Problem connecting to Private APN

Hi, thanks for keeping us posted.

Bill