Search found 735 matches

by bill.yu
Wed Sep 19, 2018 10:18 am
Forum: ReSpeaker
Topic: Getting microphone direction using C++
Replies: 1
Views: 724

Re: Getting microphone direction using C++

Hi there,

please refer to http://respeaker.io/librespeaker_doc/. thanks.

best rgds
Bill
by bill.yu
Tue Sep 18, 2018 8:00 pm
Forum: Wio Series
Topic: Wio Tracker - recognized under Other devices
Replies: 3
Views: 1882

Re: Wio Tracker - recognized under Other devices

Hi Gabrijel I see the same issue on win7. I solved the issue with below instructions.  1. follow http://wiki.seeedstudio.com/Seeed_Arduino_Boards/ to install wio gps tracker into board manager 2. then open the arduio ide, click file-->preferences--> click the link as below picture https://seeed.user...
by bill.yu
Tue Sep 18, 2018 7:54 pm
Forum: ReSpeaker
Topic: ReSpeaker 4-Mic Linear Array Kit Channel Position Problem.
Replies: 9
Views: 2279

Re: ReSpeaker 4-Mic Linear Array Kit Channel Position Problem.

Hi there

we use s32_le in test. thanks.

Bill
by bill.yu
Tue Sep 18, 2018 7:44 pm
Forum: ReSpeaker
Topic: Windows IOT
Replies: 1
Views: 564

Re: Windows IOT

Hi Carl,

the pi hat mics do not support win10 iot yet. we have the mic array v2.0 can support mac, linux. windows. for more info, please refer to http://wiki.seeedstudio.com/ReSpeaker_Mic_Array_v2.0/. thanks.

best rgds
Bill
by bill.yu
Tue Sep 18, 2018 7:41 pm
Forum: Grove
Topic: 128x128 oled
Replies: 9
Views: 2313

Re: 128x128 oled

Hi there,

Sorry, i missed the message. do you use https://github.com/Seeed-Studio/OLED_Di ... SH1107G_v2 examples? thanks.

best rgds
Bill
by bill.yu
Tue Sep 18, 2018 7:36 pm
Forum: Grove
Topic: Problems with Grove Multichannel Gas Sensor
Replies: 3
Views: 939

Re: Problems with Grove Multichannel Gas Sensor

Hi Cesar

I see you pull up a resistor on the scl and sda. we have already pulled 10k on grove-multichannel gas sensor. pls try to remove and see any improvement. thanks.

Bill
by bill.yu
Tue Sep 18, 2018 7:32 pm
Forum: Grove
Topic: grove gsr on grovepi
Replies: 8
Views: 1823

Re: grove gsr on grovepi

Hi Joe Step 1. Follow Setting Software to configure the development environment. https://www.dexterindustries.com/GrovePi/get-started-with-the-grovepi/setting-software/ Step 2. Git clone the Github repository. cd ~ git clone https://github.com/DexterInd/GrovePi.git Step 3. Excute below commands to u...
by bill.yu
Mon Sep 17, 2018 12:45 pm
Forum: Grove
Topic: grove gsr on grovepi
Replies: 8
Views: 1823

Re: grove gsr on grovepi

HI Joe,

it is the same, coz both switch and gsr are anlog sensor. so you can use the same script to extract the analog reading. thanks.

best rgds
Bill
by bill.yu
Mon Sep 17, 2018 11:57 am
Forum: Shields
Topic: I am looking for the identification of pins for the "2.8 TFT
Replies: 1
Views: 31410

Re: I am looking for the identification of pins for the "2.8 TFT

Hi there, here are the pin map and the pins we used for the tft. thanks. Digital Pins Pin Name Function D0 NOT USED D1 NOT USED D2 NOT USED D3 NOT USED D4 TF_CS D5 TFT_CS D6 TFT_DC D7 BACKLIGHT(Selectable) D8 NOT USED D9 NOT USED D10 NOT USED D11 SPI_MOSI D12 SPI_MISO D13 SPI_SCK Analog Pins Pin Nam...
by bill.yu
Mon Sep 17, 2018 11:50 am
Forum: To Be Classified
Topic: Beamforming to specific angle - MicArray V2
Replies: 1
Views: 1157

Re: Beamforming to specific angle - MicArray V2

Hi Miguel We can use the jtag port at back side to burn the image, but you have the write the code. sorry, we do not open source the firmware source code. thanks. https://github.com/SeeedDocument/forum_doc/raw/master/image/jtag_1.png https://github.com/SeeedDocument/forum_doc/raw/master/image/jtag_2...