Search found 732 matches

by bill.yu
Thu Sep 19, 2019 11:22 am
Forum: Grove
Topic: LED Strip Driver not working with Wio LTE Tracker
Replies: 3
Views: 470

Re: LED Strip Driver not working with Wio LTE Tracker

Hi there~

1. If you connect to D38, then you have to define the CLK and DIO as 38 and 39.

2. What kinds of LED do you use? thanks.
by bill.yu
Mon Sep 16, 2019 10:21 am
Forum: Grove
Topic: Grove board for programming ICs
Replies: 1
Views: 560

Re: Grove board for programming ICs

Hi there~

Please  see below replies. Hope it helps. 

1. All the grove modules work with Base shield v2.0.

2. For use the uno to program the  ATTiny85 , you can refer to below link.
https://create.arduino.cc/projecthub/ar ... uno-afb829  
by bill.yu
Wed Sep 11, 2019 3:02 pm
Forum: ReSpeaker
Topic: one of tracks is mute always (newbie)
Replies: 2
Views: 621

Re: one of tracks is mute always (newbie)

Hi there~ The channel 5 is playback channel. if you plug the mic array v2.0 to PC and then you select mic array v2.0 as audio output device, you can see the data on channel 5. thanks. Channel 0: processed audio for ASR Channel 1: mic1 raw data Channel 2: mic2 raw data Channel 3: mic3 raw data Channe...
by bill.yu
Tue Sep 10, 2019 2:31 pm
Forum: BeagleBone
Topic: RISK unknown to Power BBG from micro-USB w/ only +5V and ground
Replies: 4
Views: 1218

Re: RISK unknown to Power BBG from micro-USB w/ only +5V and ground

Hi there~

You can power the BBG with 5V and GND directly without the D+/D-. You can add the fuse for protection, thanks.
by bill.yu
Tue Sep 10, 2019 2:21 pm
Forum: Wio Series
Topic: Wio Lite W600
Replies: 5
Views: 865

Re: Wio Lite W600

Hi there~

For the library, there is issue with codes. Sorry for the inconvenience. We will update soon. Keep you posted. thanks.
by bill.yu
Tue Sep 10, 2019 2:07 pm
Forum: Wio Series
Topic: Wio Lite MG126 - errors when compiling
Replies: 5
Views: 518

Re: Wio Lite MG126 - errors when compiling

Hi there~ If you do not use the bluetooth, you have to change the platform.txt as below.thanks. recipe.c.combine.pattern="{compiler.path}{compiler.c.elf.cmd}" "-L{build.path}" {compiler.c.elf.flags} {compiler.c.elf.extra_flags} "-T{build.variant.path}/{build.ldscript}" "-Wl,-Map,{build.path}/{build....
by bill.yu
Tue Sep 10, 2019 1:59 pm
Forum: ReSpeaker
Topic: What is the unit of data?
Replies: 2
Views: 544

Re: What is the unit of data?

Hi there~

Please let us know which product and provide more info. thanks.
by bill.yu
Mon Sep 09, 2019 4:47 pm
Forum: BeagleBone
Topic: RISK unknown to Power BBG from micro-USB w/ only +5V and ground
Replies: 4
Views: 1218

Re: RISK unknown to Power BBG from micro-USB w/ only +5V and ground

Hi there~

We can not see the picture, can you post once again, please? thanks.
by bill.yu
Mon Sep 09, 2019 4:44 pm
Forum: Wio Series
Topic: Wio Lite W600
Replies: 5
Views: 865

Re: Wio Lite W600

Hi there~

Do you talk about the win7/8 usb driver? The software team is looking @ the issue, Keep you posted. thanks.
by bill.yu
Mon Sep 09, 2019 4:43 pm
Forum: Wio Series
Topic: Wio Lite MG126 - errors when compiling
Replies: 5
Views: 518

Re: Wio Lite MG126 - errors when compiling

Hi there~ Please refer to step 4 of the software session of wiki page. thanks. http://wiki.seeedstudio.com/Wio-Lite-MG126/#software 1. Open the platform.txt file in the folder: C:\Users\$(USER_NAME)\AppData\Local\Arduino15\packages\Seeeduino\hardware\Seeeduino_Wio_Lite_BLE\1.0.0\platform.txt 2. Go t...