Search found 735 matches

by bill.yu
Fri Sep 27, 2019 10:27 am
Forum: ReSpeaker
Topic: Respeaker mic array v2 AEC and sdk
Replies: 1
Views: 577

Re: Respeaker mic array v2 AEC and sdk

Hi there~

For AEC parameters, there are some parameters that you can adjust at below link.
For the firmware customization, you can drop mail to techsupport@seeed.cc. thanks.

http://wiki.seeedstudio.com/ReSpeaker_M ... _v2.0/#faq
by bill.yu
Fri Sep 27, 2019 10:21 am
Forum: ReSpeaker
Topic: Respeaker / MacMini / Siri
Replies: 1
Views: 330

Re: Respeaker / MacMini / Siri

Hi there~

Do you mean respeaker mic array v2.0? It uses UAC1.0. You can connect to any Mac versions. Hope it helps. thanks.
by bill.yu
Fri Sep 27, 2019 10:18 am
Forum: Shields
Topic: CAN Bus shield 2.0 OBD Jumpers
Replies: 6
Views: 843

Re: CAN Bus shield 2.0 OBD Jumpers

Hi Alex~

You do not need to cut the pads, you just need to connect the ODBII and DB9 directly. thanks.

Image
Image
by bill.yu
Thu Sep 26, 2019 4:28 pm
Forum: Arduino & Seeeduino
Topic: Debugging Maixduino?
Replies: 1
Views: 596

Re: Debugging Maixduino?

Hi there~

If the JTAG pins aren't accessible through headers, it is possible that jumpers may solve the problem. If this problem still exists, you can also ask Sipeed support team at sipeed@support.com for advanced information.

Thanks cheers,
JL from Seeed.
by bill.yu
Thu Sep 26, 2019 3:43 pm
Forum: Grove
Topic: Grove Selection Guide - Feed-back
Replies: 1
Views: 960

Re: Grove Selection Guide - Feed-back

Hello~

Thank you so much for your suggestions!

We have received your advice and fed them back to our team and we will soon update it.

By the way, this is the address of compatibility list:
https://www.seeedstudio.com/compatibility-list.html

Thanks sincerely,
JL from Seeed
by bill.yu
Thu Sep 26, 2019 3:21 pm
Forum: Grove
Topic: Grove Base Hat Zero
Replies: 4
Views: 652

Re: Grove Base Hat Zero

Hi there~ According to you description, we advise you to reburn the firmware via SWD port. The address of firmware file (.zip) is: https://github.com/SeeedDocument/Grove_Base_Hat_for_Raspberry_Pi/raw/master/res/grove_rpi_base_hat-v0.2-20180905-02.zip Download it and see if it works. If you have any ...
by bill.yu
Thu Sep 26, 2019 2:46 pm
Forum: Grove
Topic: Voltaje divider supply
Replies: 3
Views: 401

Re: Voltaje divider supply

Hi there ~

The range of working Voltage of Grove Voltage Divider is from 4.7 to 5.3v, so you can not use the battery.
This is the specification of the voltage divider.

Image

Thanks cheers
JL
by bill.yu
Tue Sep 24, 2019 5:58 pm
Forum: General Info - Guidance
Topic: Pi Zero Solar Power - Noob Questions
Replies: 1
Views: 1307

Re: Pi Zero Solar Power - Noob Questions

Hi there~ The main concern is that the power consumption of the pi zero and camera. The pi zero idle power consumption is around 80ma. You had better to add the cirucit to detect the battery voltage and power on/off the raspberry pi zero. You also have to calculate the solar panel size and battery c...
by bill.yu
Tue Sep 24, 2019 5:46 pm
Forum: General Info - Guidance
Topic: cheapers IoT with 4G module
Replies: 1
Views: 1198

Re: cheapers IoT with 4G module

Hi there~

You can conside to use the wio lte cat1 or nbiot. thanks.

http://wiki.seeedstudio.com/Wio_LTE_Cat.1/
http://wiki.seeedstudio.com/Wio_LTE_Cat ... T_Tracker/
by bill.yu
Tue Sep 24, 2019 5:44 pm
Forum: Grove
Topic: Grove NFC v1.1 does not work with UART
Replies: 19
Views: 2973

Re: Grove NFC v1.1 does not work with UART

Hi there~

It looks like the rx/tx is occupied by the bluetooth module. You can use the software serial to communicate with NFC. thanks.