Search found 98 matches

by Icing
Wed Mar 10, 2010 10:04 am
Forum: To Be Classified
Topic: RFBee
Replies: 1
Views: 2223

Re: RFBee

Dear Seeedstudio Please publish the firmware used on the board. I would like to develop a small usb fob for the cc1101 and stay compatible to your solution. Cheers Rubi Hi Rubi, You can find the download link in the datasheet of RFBee, or download them directly from here. RFBee firmware v1.0: http:...
by Icing
Fri Jan 22, 2010 10:29 am
Forum: To Be Classified
Topic: bluetooth relay driver project
Replies: 2
Views: 3130

Re: bluetooth relay driver project

The voltage used by bluetooth module is between 2.7v-4.2v, so its output could not get 9v. The module hasn't DTR port, it use Tx and Rx to send or receive data from other bluetooth. The CTS and RTS port is controlled by the module itself as the indication for the user, but they could not controlled ...
by Icing
Fri Dec 25, 2009 9:28 am
Forum: DSO
Topic: Unsuccessful Nano code compilation
Replies: 11
Views: 9219

Re: Unsuccessful Nano code compilation

Try to do changes in stm32f10x_vector.c as follows: //void __program_start( void ); //this is for IARv4 void __iar_program_start( void );// this if for IARv5 //#pragma location = "INTVEC" // this is for IARv4 #pragma location = ".intvec" // this is for IARv5 /* STM32F10x Vector Table entries */ cons...
by Icing
Wed Dec 16, 2009 9:04 am
Forum: To Be Classified
Topic: Shield needed for Seeeduino Mega board
Replies: 5
Views: 3608

Re: Shield needed for Seeeduino Mega board

We have finished the prototype,and you can get it in the near future.

-Icing
by Icing
Wed Dec 16, 2009 8:49 am
Forum: Fusion PCB/ PCBA Services
Topic: when is the 4x4 cube coming out?
Replies: 2
Views: 2863

Re: when is the 4x4 cube coming out?

It may come out next week.
by Icing
Wed Dec 02, 2009 9:19 am
Forum: DSO
Topic: Third-party Firmware for DSO Nano
Replies: 8
Views: 11251

Re: Third-party Firmware for DSO Nano

To be able to recover the firmware,you can firstly upload the original pre-installed in the DSO.
by Icing
Thu Nov 26, 2009 4:56 pm
Forum: To Be Classified
Topic: Knob for rotary encoder
Replies: 1
Views: 2244

Re: Knob for rotary encoder

Thanks,Oracle.
We'll consider them as soon as possible.
by Icing
Thu Nov 26, 2009 4:05 pm
Forum: To Be Classified
Topic: Plastic rivets in harness kit are very tight
Replies: 1
Views: 1836

Re: Plastic rivets in harness kit are very tight

Thanks for your suggestion, we'll make it longer in after.