Search found 98 matches

by Icing
Sun Aug 15, 2010 11:09 am
Forum: To Be Classified
Topic: RFBee firmware updating
Replies: 143
Views: 108461

Re: RFBee firmware updating

Hi Hans,

I also notice that it is nonsense of IDLE mode, and it's more compact to keep TRANSMIT_MODE, RECEIVE_MODE, TRANSCEIVE_MODE, LOWPOWER_MODE. And SLEEP_MODE can also be removed as there's no ATMD5, with ATSL instead.

Regards,

-Icing
by Icing
Fri Jul 30, 2010 10:53 pm
Forum: Bee series & WSN
Topic: Bluetooth Bee PIO1
Replies: 3
Views: 3090

Re: Bluetooth Bee PIO1

Hi, How is the timing in relation to the status-code message? Can I assume that the module always sends the status-change message before changing PIO1 to high (when connected) and after changing to low (when disconnected)? Yes, the module will return the status message while in different sate, howev...
by Icing
Tue Jul 27, 2010 9:48 pm
Forum: Bee series & WSN
Topic: Bluetooth Bee Control IO Pins
Replies: 2
Views: 2474

Re: Bluetooth Bee Control IO Pins

Hi, Actually, the PIOs of the Bluetooth Bee are could not controlled by the user excepting the PIO0, PIO1, PIO10 and PIO11 of which the function is described on the datasheet. The profile of the Buletooth Bee is SPP, so you can just communicate between your smartphone and the Bee through an serial t...
by Icing
Mon Jul 26, 2010 12:50 am
Forum: Arduino & Seeeduino
Topic: Teething problems with Stalker
Replies: 5
Views: 3143

Re: Teething problems with Stalker

Hi Tony,

The stability of filelogger lib is not very well on stalker.
You may try the lib in the following link:
http://code.google.com/p/fat16lib/

Regards,

-Icing
by Icing
Sun Jul 25, 2010 10:10 am
Forum: To Be Classified
Topic: RFBee firmware updating
Replies: 143
Views: 108461

Re: RFBee firmware updating

Hi rich,

Thanks for your updating.

The PC0~PC5 and ADC7 should be all analog inputs, except the PC6 which is not lay out.

The I2C is also available as they are multi-used with PC4 and PC5.

Regards,

-Icing
by Icing
Sat Jul 17, 2010 2:02 am
Forum: To Be Classified
Topic: RFBee firmware updating
Replies: 143
Views: 108461

Re: RFBee firmware updating

HI Hans,

Thanks for your updating!

The CRC is ok now, and there's no garbage any more. :)

I have one question to ask:
In the latest verison, When the Arduino on RFBee is in sleep mode, what's the condition that will wake it up?

Thank you,

-Icing
by Icing
Fri Jul 16, 2010 1:54 am
Forum: Arduino & Seeeduino
Topic: How to use source driver channel?
Replies: 2
Views: 2315

Re: How to use source driver channel?

I read in the panel the 8 source driver channel Rainbowduino feature, but how to use it?
What do you want to do with the Rainbowduino?
by Icing
Thu Jul 15, 2010 11:47 pm
Forum: Arduino & Seeeduino
Topic: Seeeduino Stalker Tutorial?
Replies: 8
Views: 5611

Re: Seeeduino Stalker Tutorial?

Hi Ed, To upload a basic blink sketch, please try to do as follows: 1. connect UartSB to stalker; 2. move switches on UartSB to xbee and 5v side; move switch on stalker to on(top) side. 3. connect UartSB to PC. 4. Open Arduino 0018 and open the Digital->Blink sketch; 5. Choose the Board of "Arduino ...
by Icing
Thu Jul 15, 2010 11:13 pm
Forum: Bee series & WSN
Topic: Set up connections between two BluetoothBee step by step
Replies: 38
Views: 91678

Re: Set up connections between two BluetoothBee step by step

I need to set the module as master! The module could not be searched when in master mode. So you must set it to slave. I have another problem! How can the master connect with 2 or more slaves ?? The master moulde can only connect to one slave at a time. If i connect to one slave if i try the +conn,...
by Icing
Mon Jul 12, 2010 9:30 pm
Forum: Bee series & WSN
Topic: Set up connections between two BluetoothBee step by step
Replies: 38
Views: 91678

Re: Set up connections between two BluetoothBee step by step

How can i put the master device in discoverable mode? Try to make the buletooth module as a slave by using command \r\n+STWMOD=0\r\n; Then make the module be inquiredable \r\n+INQ=0\r\n, At this point, your pc should find the buletooth device! May this helpful to you, and feel free to ask any quesi...