Search found 305 matches

by kavi
Tue Dec 09, 2014 8:16 pm
Forum: Shields
Topic: TFT V2.0 SHIELD , Pinout NAMES .
Replies: 6
Views: 7026

Re: TFT V2.0 SHIELD , Pinout NAMES .

Thank you for purchasing the TFT Shield. Have you seen the EAGLE schematic and board files mentioned in Wiki->TFT Touch Shield v2.0

Let me know if you need any other clarification. Thanks
by kavi
Tue Dec 09, 2014 7:05 pm
Forum: Shields
Topic: How to get the Arduino design a Plastic or Metal shell?
Replies: 1
Views: 687

Re: How to get the Arduino design a Plastic or Metal shell?

You can try 3D printing services or acrylic laser cutting services for a prototype shell.There are few standard sized plastic or aluminium cases available.Search for "case" in seeed bazzar.

Thanks
by kavi
Tue Dec 09, 2014 3:14 pm
Forum: Arduino & Seeeduino
Topic: LCD108B6B
Replies: 1
Views: 1126

Re: LCD108B6B

LCD108B6B has HD44780 interface/ driver chip. It can be programmed like any other 16x2 HD44780 based LCDs. We do not have a specfic example for Raspberry Pi. But, searching for "Rasberry Pi + HD44780 LCD" produces many examples by the community.

Thanks.
by kavi
Tue Dec 09, 2014 2:57 pm
Forum: Arduino & Seeeduino
Topic: How to power a Seeeduino Stalker v2.3 - water proof
Replies: 2
Views: 1745

Re: How to power a Seeeduino Stalker v2.3 - water proof

Sorry for the delayed reply. Seeeduino Stalker uses CN3063 for charging the LiPo using Solar cell. You need to take care of CN3063 specification to fullfil the requirements of your application. 1)Use a 5V DC power supply or charger. 2)If you have a 9v, 1A charger. Use a 5V fixed linear voltage regul...
by kavi
Tue Dec 09, 2014 2:25 pm
Forum: Arduino & Seeeduino
Topic: Seeeduino Stalker v3 data flash
Replies: 2
Views: 1746

Re: Seeeduino Stalker v3 data flash

Yes.Seeeduino Stalker v3 uses ATMega328 which has an internal EEPROM of 1K.For larger data use external SD card.

Thanks