Search found 305 matches

by kavi
Thu Apr 21, 2016 6:17 pm
Forum: Xadow Pebble
Topic: Does not work
Replies: 16
Views: 22122

Re: Does not work

There is a software update in Xadow GPS V2 please find it in the followinglink
by kavi
Thu Apr 21, 2016 6:00 pm
Forum: Wearables
Topic: Xadow GPS v2 Returning 0 for both LAT and Long
Replies: 1
Views: 3141

Re: Xadow GPS v2 Returning 0 for both LAT and Long

Sorry for the delayed answer do you still have this issue.If so please send the details to tickets@seeed.uservoice.com
by kavi
Thu Apr 21, 2016 5:55 pm
Forum: Grove
Topic: [error] Grove Gesture Sensor
Replies: 3
Views: 2333

Re: [error] Grove Gesture Sensor

Yes the gesture sensor should trigger an event.Please find the following wiki documentation page to know more about this sensor.
by kavi
Thu Apr 21, 2016 1:33 pm
Forum: Xadow Pebble
Topic: Does not work
Replies: 16
Views: 22122

Re: Does not work

We are sorry for the inconvenience caused please write about your issue in detail with photograph of your experimental setup to tickets@seeed.uservoice.com
by kavi
Wed Apr 20, 2016 7:35 pm
Forum: Grove
Topic: [question] Grove Analog Servo only has 8 angles?
Replies: 2
Views: 1842

Re: [question] Grove Analog Servo only has 8 angles?

Hi,

The servo moves 1° per step from 0-180° using the sweep example in the Arduino IDE.It is tested with Arduino .

Thanks and Regards
by kavi
Wed Apr 20, 2016 6:01 pm
Forum: Grove
Topic: [QUESTION] Piezo Vibration Sensor
Replies: 1
Views: 1841

Re: [QUESTION] Piezo Vibration Sensor

Hello, Grove-Piezo Vibration sensor outputs HIGH when vibration is detected and LOW when no vibration are detected.The sensitivity can be adjusted by varying the POT. This module processes the output from the Piezo vibration sensor using LM293D The video links that you have mentioned in your post se...
by kavi
Tue Apr 19, 2016 8:00 pm
Forum: Grove
Topic: Grove water sensor
Replies: 3
Views: 1774

Re: Grove water sensor

Hi, We wrote a small example program for PIC void main() { PORTC=0; //initialize portc TRISC=0x07; //configure portc (RC7 to RC3) as output and (RC2 to RC0 as input) ANSELH=0; //configure an pin as digital I/O ANSEL=0; while(1){ //connect the grove water sensor sig to PIN RC0,RC1 and RC2( you need a...
by kavi
Tue Apr 19, 2016 7:41 pm
Forum: Shields
Topic: GPRS Shield v3 questions
Replies: 3
Views: 3096

Re: GPRS Shield v3 questions

1.The difference between Gprs Shiled v2.0 and the Gprs Shiled v3.0 is change in the arduino socket to the latest Arduino Uno standard. Except this, all the features are same with the Gprs Shiled v2.0. 2.Already the JMP pads are connected to the GPRS shield v3.0.So, you don't need to solder it separa...
by kavi
Fri Apr 15, 2016 1:31 pm
Forum: Grove
Topic: [Question] Grove Indoor Environment kit wrong sensor values
Replies: 8
Views: 6468

Re: [Question] Grove Indoor Environment kit wrong sensor val

Please follow the steps below
  • 1.Delete the existing library from the Arduino IDE 1.6.7
    2.Include the new zip file in Arduino IDE 1.6.8.
    3.Compile the code in the new IDE.
and Let us know if you have any issues.

Thanks and Regards
by kavi
Fri Apr 08, 2016 5:38 pm
Forum: Xadow Pebble
Topic: Does not work
Replies: 16
Views: 22122

Re: Does not work

Xadow GPS should be working well in outdoors in open air