Search found 305 matches

by kavi
Tue Mar 10, 2015 5:14 pm
Forum: Grove
Topic: Multiple Ultrasonic Sensors
Replies: 4
Views: 2456

Re: Multiple Ultrasonic Sensors

Hi,

Yes, you can connect another ultrasonic sensor in D3 and in D4 provided you make changes in the program also.

Please let us know if you have any other queries.

Thanks
by kavi
Tue Mar 10, 2015 4:47 pm
Forum: Arduino & Seeeduino
Topic: Seeduino lotus
Replies: 3
Views: 1398

Re: Seeduino lotus

Yes,

The size of Stalker V3 is 86.74mm x 60.96mm, and it can be put inside the plastic enclosure of V2.3 which is of dimensions 50 (H) x 68 (W) x 100 (D) (mm)

Thank you
by kavi
Thu Mar 05, 2015 3:49 pm
Forum: Grove
Topic: Grove HCHO Sensor Suggested Improvement
Replies: 2
Views: 1477

Re: Grove HCHO Sensor Suggested Improvement

Thanks for your suggestion.
by kavi
Wed Feb 25, 2015 6:41 pm
Forum: Arduino & Seeeduino
Topic: Seeeduino ADK and "OSCOKIRQ failed to assert" error
Replies: 12
Views: 9985

Re: Seeeduino ADK and "OSCOKIRQ failed to assert" error

Hi,

Have you tried the above solutions to this problem?

If it still does not work, please let us know. I will redirect your query to our internal team to check if it is a hardware issue.

Thanks
by kavi
Wed Feb 25, 2015 6:28 pm
Forum: Grove
Topic: SD CARD writing
Replies: 1
Views: 980

Re: SD CARD writing

Hi,

1.Please upload a photo of your hardware setup.

2.What SD card are you using (Type,Make,Size)?

Thank you
by kavi
Mon Feb 23, 2015 5:02 pm
Forum: Grove
Topic: error on serial lcd version 0.9
Replies: 4
Views: 2672

Re: error on serial lcd version 0.9

Hi,

Yes,It is possible to use grove and some sensors in breadboard simultaneously but make sure same pin is not used more than once.

Yes ,the 5V and GND can be normally used.


Thank you
by kavi
Fri Feb 13, 2015 5:08 pm
Forum: Shields
Topic: Charging Arduino from solar battery
Replies: 5
Views: 3670

Re: Charging Arduino from solar battery

Hello,

Seeeduino Stalker V3.0(or) Wireless sensor node-Solar Kit(or) LiPo rider Pro with arduino compatible board may be used to implement your application.

These might not fit your size requirements.

Thanks.
by kavi
Fri Feb 13, 2015 3:25 pm
Forum: Shields
Topic: TFT Touch Shield V1.0 with Leonardo?
Replies: 2
Views: 1859

Re: TFT Touch Shield V1.0 with Leonardo?

Hello, Could you please check if the example code mentioned in http://www.seeedstudio.com/wiki/2.8''_TFT_Touch_Shield_V1.0 . It looks like the necessary pin re-mapping for Leonardo is mentioned in that code : #elif defined(__AVR_ATmega32U4__) // leonardo #define YP A2 // must be an analog pin, use "...
by kavi
Fri Feb 13, 2015 3:18 pm
Forum: Grove
Topic: Grove - I2C Color Sensor - Raw RGB to 255 RGB
Replies: 1
Views: 946

Re: Grove - I2C Color Sensor - Raw RGB to 255 RGB

Hello, "Grove - I2C Color Sensor" should work similarly irrespective of VCC voltage -- 3.3v or 5V. The design includes a LDO and Logic level converter to adapt to two different VCC voltages. In the example code, the raw colour information is presented in int format. Please scale it down to 0-255 by ...
by kavi
Fri Feb 13, 2015 3:03 pm
Forum: Arduino & Seeeduino
Topic: Can RF​​μ-328-BARE be replaced by XRF wireless RF?
Replies: 1
Views: 962

Re: Can RF​​μ-328-BARE be replaced by XRF wireless RF?

Hello, "XRF wireless RF radio UART serial data module XBee shaped" which uses CC1110 is a radio module and does not come with Atmega328. This module can be used with existing Arduino using UART interface. We have many RF(ISM), Xbee, WiFi based products(http://www.seeedstudio.com/depot/Communication-...