Search found 34 matches

by philip.mallon
Thu Apr 28, 2016 3:13 pm
Forum: Wio Series
Topic: [idea] Garage parking assistance
Replies: 3
Views: 2876

Re: [idea] Garage parking assistance

This is a great idea and well done. We have one that uses laser guidance for the driver in the garage and it senses the car by heat. On a cold day it does not work so we may try your construction. We think it is one of the best gadgets in the house. Is the range of the ultrasonic sensor too short?
by philip.mallon
Wed Apr 27, 2016 6:42 pm
Forum: Wio Series
Topic: ThingSpeak:Data Collect & Analysis for Wio Link
Replies: 3
Views: 4245

Re: ThingSpeak:Data Collect & Analysis for Wio Link

Yesterday i received my Deluxe pack from Kickstarter and connected the air quality sensor to initial state (with ifttt & maker channel) What I want is to control my data for days by using the ThingSpeak platform which is open source. Does anyone knows how to do it or can help?it would be a great id...
by philip.mallon
Wed Apr 27, 2016 12:28 pm
Forum: Wio Series
Topic: #Discussion#Wio Link Server document has released, then?
Replies: 4
Views: 2323

Re: #Discussion#Wio Link Server document has released, then?

Hi philip, Python version is fine. The problem is your earlier installation is still running (at the same machine), and listening at port 8080. Unfortunately 8080 is used by lean server too. The full function server has "data exchange function" as well, so we assume that there is no need to deploy ...
by philip.mallon
Wed Apr 27, 2016 7:44 am
Forum: Wio Series
Topic: #Discussion#Wio Link Server document has released, then?
Replies: 4
Views: 2323

Re: #Discussion#Wio Link Server document has released, then?

Installed the Lean Server but get error: "socket.error: [Errno 98] Address already in use" when running either on or off line versions. What could be causing this error. When thru the install procedure and all when ok there. The rest of the Traceback is: Traceback (most recent call last): File "./se...
by philip.mallon
Wed Apr 27, 2016 7:40 am
Forum: Wio Series
Topic: #idea Air Quality and UV Index Measurements
Replies: 3
Views: 2810

Re: #idea Air Quality and UV Index Measurements

eberstein wrote:What are those graphing tools you use in the last picture? I've seen them a lot but cannot find them..
H ebersteini, the graphing tools are part of the node-red library ui node (user interface). Get them at: http://flows.nodered.org/node/node-red-contrib-ui
by philip.mallon
Sun Apr 24, 2016 9:59 am
Forum: Grove
Topic: Reliability of Grove Modules
Replies: 0
Views: 1515

Reliability of Grove Modules

Hello, I purchased hundreds of Grove modules but I am just starting to use them on projects. I am using 10 Grove modules on WioLink computers and have found that both the Grove Recorder and Grove uv sensor are unreliable. On the uv sensor the readings are jumping all over the place (see photo below)...
by philip.mallon
Sat Apr 23, 2016 9:29 am
Forum: Wio Series
Topic: Solar charger and battery
Replies: 2
Views: 1553

Re: Solar charger and battery

seeedstudio201413 wrote:Got the kits thank you! What do you guys recommend to allow me to add a solarpanel with charger and battery?
Hi nevillekong , I am preparing to do this and some related discussion is on my posting "WioLink power charging specs". When I am finished preparing I will write it up as a recipe.
Philip
by philip.mallon
Fri Apr 22, 2016 2:56 pm
Forum: Grove
Topic: UV Sensor
Replies: 2
Views: 2706

Re: UV Sensor

Thanks for your feedback. Our engineer will have a check and put a conclusion here later. Jacket Hello Jacket, I am preparing a recipe on WioLink application using this sensor - have already posted part of it on the WioLink forum. I am having a similar problem getting higher than expected values fo...
by philip.mallon
Fri Apr 22, 2016 12:00 pm
Forum: Wio Series
Topic: WioLink power charging specs
Replies: 1
Views: 882

WioLink power charging specs

I am interested in outdoor applications for Wio. I plan to used both solar and Li ion batteries. Does the Wio have voltage protection on its charging circuit? Is it possible to connect the JST 2 connector directly to a solar panel bearing in mind that solar panels even at a nominal 5V can result in ...
by philip.mallon
Fri Apr 22, 2016 9:16 am
Forum: Wio Series
Topic: Posting more than 1 digit to grove digital display
Replies: 2
Views: 6756

Re: Posting more than 1 digit to grove digital display

Hello Mark, did you get an answer to this yet? I have developed a Thermostat which uses the 4 digital digital display to display on all 4 digits and uses the ":' in the middle. My project displays" "TT:HH" for measured temperature and humidity and "TTSS" for measured temperature and set point temper...