Search found 50 matches
- Wed Mar 04, 2015 10:09 am
- Forum: Shields
- Topic: Bluetooth Shield SLD63030P
- Replies: 0
- Views: 1047
Bluetooth Shield SLD63030P
I tried to connect it via Arduino (pin default is 1234) but the sketch I used to always false (blueToothSerial.available ()). Will you help me figure out where I wrong? Thank You. #include //Software Serial Port #define RxD 6 #define TxD 7 #define DEBUG_ENABLED 1 SoftwareSerial blueToothSerial(RxD,...
- Sat Feb 07, 2015 1:32 pm
- Forum: Shields
- Topic: XBee shield with XBee
- Replies: 6
- Views: 6740
Re: XBee shield with XBee
Hi, so you would like to use Arduino board a USB to serial convert board. In this case, it should work by "XBee" -> "XBee shield" -> "Arduino UNO" -> "USB cable" -> "XCTU". But Hardware Serial (D0&D1) on Arduino UNO should be connected to XBee. Upload a empty code to Arduino UNO. Set the jumper hats...
- Thu Feb 05, 2015 6:29 pm
- Forum: Shields
- Topic: XBee shield with XBee
- Replies: 6
- Views: 6740
Re: XBee shield with XBee
Hi, I think the real question is : Can I use XCTU with and xbee on a xbee shield which one is on an arduino connected to my PC trough USB ? Xbee -> xbeeshield -> arduino -> usb -> PC -> XCTU => will it work ? Because in my case, it's been more than one week that I'm trying to make this set to work ...
- Tue Feb 03, 2015 6:49 pm
- Forum: LinkIt
- Topic: Is the Grove Dust Sensor compatible to the LinkIt One board
- Replies: 0
- Views: 1231
Is the Grove Dust Sensor compatible to the LinkIt One board
I would like to ask if the Grove Dust Sensor: SEN12291P is directly interfaceable to the LinkIt One board? I saw that its also included on the Grove Starter Kit for the LinkIt One but the datasheet shows that its voltage output is 4v and is beyond the 3.3v limit of the LinkIt One GPIO. I would like...
- Mon Feb 02, 2015 5:58 pm
- Forum: Shields
- Topic: Is CAN shield compatible with the Arduino Ethernet shield
- Replies: 0
- Views: 1133
Is CAN shield compatible with the Arduino Ethernet shield
is seeedstudio can bus shield compatible with the Arduino Ethernet shield Hi, CAN Bus shield and Arduino Ethernet shield both use SPI for communication with Arduino board. Thus, they cannot be used at the same time. CAN Bus shield takes D9/D10(selectable) as SS pin. Arduino Ethernet shield takes D1...
- Mon Feb 02, 2015 5:20 pm
- Forum: Shields
- Topic: XBee shield with XBee
- Replies: 6
- Views: 6740
XBee shield with XBee
i could not detect my xbee using seeeds xbee shield v2.1.....shield was connected to arduino......but my XCTU is detecting arduino but not xbee using shield...........do i need to install any drivers for shield Hi, XCTU can be used to configure XBee module if it is connected to PC via a XBee adapto...
- Mon Feb 02, 2015 3:35 pm
- Forum: Grove
- Topic: fingerprint sensor dead?
- Replies: 0
- Views: 1104
fingerprint sensor dead?
i've received a grove fingerprint sensor from you. I try to get it working, but no chance. I checked it with a seeeduino lotus, with a stalker and a base shield, and with a xbee carrier, all withnthe same result: the sensor blinks one on powerup, but if i' running enroll.ino i only get the output t...
- Fri Jan 30, 2015 2:47 pm
- Forum: Shields
- Topic: Wifi Shield is compatible with Arduino Due
- Replies: 0
- Views: 1725
Wifi Shield is compatible with Arduino Due
Wifi Shield which prices $39.95 is compatible with Arduino due? Wifi shield (SKU:WLS06201P) can work with Arduino Due. On hardware, you can connect them via one of the four Serial Ports on Arduino Due(If you use Serial 1-3, you may need to make the connection with jumper wires). The current wifi sh...
- Thu Dec 25, 2014 6:44 pm
- Forum: To Be Classified
- Topic: Rainbow cube difficulties.
- Replies: 3
- Views: 10719
Re: Rainbow cube difficulties.
Hi robharrop,
I have uploaded the test code on this link: http://www.seeedstudio.com/wiki/File:Rainbowduino.zip
Please unzip this to the arduino library. Thanks!
I have uploaded the test code on this link: http://www.seeedstudio.com/wiki/File:Rainbowduino.zip
Please unzip this to the arduino library. Thanks!
- Mon Dec 22, 2014 6:24 pm
- Forum: Arduino & Seeeduino
- Topic: Stalker V3 compatibility with Same box as V2.3?
- Replies: 3
- Views: 1863
Re: Stalker V3 compatibility with Same box as V2.3?
Does the Stalker V3 which has a different board shape, without the corner cutouts and a little shorter than the V2.3 , fit in the plastic box you have been selling for V2.3? Hi mholler, Thanks for your question! The size of Stalker V3 is 86.74mm x 60.96mm, and it can be put inside of this plastic e...