Search found 6 matches

by bleepbloop
Fri Nov 12, 2010 6:46 am
Forum: To Be Classified
Topic: Shield needed for Seeeduino Mega board
Replies: 5
Views: 3622

Re: Shield needed for Seeeduino Mega board

azuria wrote:Also, will there be a electronic brick shield for the mega?
I would love to see this. Maybe with SMT headers on the bottom to allow for more connectors along the top and bottom long sides.
by bleepbloop
Fri Nov 12, 2010 6:45 am
Forum: To Be Classified
Topic: JST connectors
Replies: 0
Views: 1679

JST connectors

Hi!

Thanks for offering this product: JST 2 Pin power connector

Can you consider labeling it as JST-XH style.

Also, I have a need for 1000+ JST-PH style cables. Would it be possible to source them from you or consider carrying them?
by bleepbloop
Fri Nov 12, 2010 6:40 am
Forum: To Be Classified
Topic: Large Image in Chrome
Replies: 2
Views: 2182

Re: Large Image in Chrome

Lightbox is broken here too in Chrome on Win 7.
Hope to see it back to normal soon. :geek:
by bleepbloop
Sun Feb 15, 2009 12:58 pm
Forum: Bee series & WSN
Topic: Ultra-Sonic Ranger - GH-311RT DATASHEET?
Replies: 14
Views: 19388

Re: Ultra-Sonic Ranger - GH-311RT DATASHEET?

I have an idea. I saw in a previous post that at 9V the range is 2.2 meters. At 5V the range is much shorter about 30 cm. Is it possible to vary the voltage to get a different threshold turn on distance? For example at 5.5V it would be 45cm 6V 50cm. I haven't tested this because I don't have a power...
by bleepbloop
Sun Feb 15, 2009 9:05 am
Forum: Bee series & WSN
Topic: Ultra-Sonic Ranger - GH-311RT DATASHEET?
Replies: 14
Views: 19388

Re: Ultra-Sonic Ranger - GH-311RT DATASHEET?

I tried the ping code today and I got the following results: 0in, 0cm 0in, 0cm 0in, 0cm 463976in, 1183939cm 0in, 0cm 1536545in, 3920839cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 312580in, 797619cm 882601in, 2252155cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0cm 0in, 0...
by bleepbloop
Fri Jan 23, 2009 3:43 am
Forum: Bee series & WSN
Topic: Ultra-Sonic Ranger - GH-311RT DATASHEET?
Replies: 14
Views: 19388

Re: Ultra-Sonic Ranger - GH-311RT DATASHEET?

Hi, according to your last reply. Does this mean that the Output is also an input like the PING module. Can the GH-311RT measure distance as well? I bought these sensors and thought that the output was analog according to distance. I realize now that this is not the case. Please verify.