Search found 7 matches

by santi3
Thu Feb 19, 2015 3:11 pm
Forum: Bee series & WSN
Topic: Configure Bluetooth Bee(Guidance)
Replies: 5
Views: 6942

Re: Configure Bluetooth Bee(Guidance)

HI,

I always used this soft in windows vista 32bits without problems. I never tested it in seven.

sorry
by santi3
Thu May 23, 2013 5:45 pm
Forum: Bee series & WSN
Topic: Configure Bluetooth Bee(Guidance)
Replies: 5
Views: 6942

Re: Configure Bluetooth Bee(Guidance)

FANTASTIC!!!

It works perfectly.

thanks so much
by santi3
Fri Jan 11, 2013 10:47 pm
Forum: Bee series & WSN
Topic: Set up connections between two BluetoothBee step by step
Replies: 38
Views: 90893

Re: Set up connections between two BluetoothBee step by step

hello everybody,

I have problems with my BluetoothBee. I followed the steps but I could not communicate correctly with my unit. I wrote a new post but nobody replied to me. anybody can help me?

http://www.seeedstudio.com/forum/viewto ... =18&t=4161

thank you
by santi3
Thu Jan 03, 2013 3:51 pm
Forum: Bee series & WSN
Topic: Configure Bluetooth Bee(Guidance)
Replies: 5
Views: 6942

Re: I can't configure Bluetooth Bee

Anybody can help me?

thanks
by santi3
Sat Dec 29, 2012 6:37 pm
Forum: Bee series & WSN
Topic: Configure Bluetooth Bee(Guidance)
Replies: 5
Views: 6942

Configure Bluetooth Bee(Guidance)

Hello Everybody, I have a problem with one bluetooth bee. I can't configure it. I use an UartSBee V4.0. I can connect with it and see some messages when device starts but I can't send any command (always returns ERROR). I tried SSCOM, hyperterm, putty and TeraTerm with the same results. How must be ...
by santi3
Fri Dec 28, 2012 8:25 pm
Forum: Shields
Topic: CAN-BUS Shield
Replies: 3
Views: 2426

Re: CAN-BUS Shield

Hi, I made one function that also can be useful for someone. maybe it also can be added to library if you think it is ok. regards, /********************************************************************************************************* ** Function name: waitingForMsg ** Descriptions: Waiting for X...
by santi3
Thu Dec 27, 2012 10:32 pm
Forum: Shields
Topic: CAN-BUS Shield
Replies: 3
Views: 2426

CAN-BUS Shield

Hi Everybody, I am using the CAN-BUS Shield with extended addresses. I found a little problem in function "mcp2515_read_id". The CAN id is calculated incorrectly (caused by the casting of the unsigned chars). I solved this issue in this way. I hope this can help other users and will be updated in th...