Search found 654 matches

by Jacket Chen
Wed May 13, 2015 12:59 am
Forum: To Be Classified
Topic: A Questionnaire survey
Replies: 1
Views: 3430

Re: A Questionnaire survey

Hi,guys here: Thanks for joining our “electric soldering iron vote” in April! Congratulations! The following 5 voters were finally selected out randomly as the lucky ones to get our Smart electric soldering iron for free trial, they are: sirhannick andreas.thorn coolgreenguy friedcircuits marcin.kli...
by Jacket Chen
Thu May 07, 2015 4:05 pm
Forum: Grove
Topic: Question regarding air quality sensor
Replies: 3
Views: 1872

Re: Question regarding air quality sensor

In fact, this sensor should be powered for more than 48 hrs before you have a test with it. Or data is useless.
by Jacket Chen
Thu May 07, 2015 3:36 pm
Forum: Arduino & Seeeduino
Topic: Stalker V3 powering on and off the SD card
Replies: 1
Views: 1384

Re: Stalker V3 powering on and off the SD card

Hi guys

Yes, it would cut off the power of SD Card while using digitalWrite(4,HIGH), and get power from battery after setting a low level to pin 4.

Read the logic level from pin4 and you can get the state of SD Card. //digitalRead(4)

Jacket
by Jacket Chen
Thu May 07, 2015 3:20 pm
Forum: Arduino & Seeeduino
Topic: Seeeduino GPRS APN
Replies: 3
Views: 3694

Re: Seeeduino GPRS APN

Try using the example sketch from Seeduino_GPRS_Master, named SIM800_Serial_Debug example. Then you could use AT commands directly and get response from Seeduino GPRS. This will help you to test a lot of parameters from your Seeduino GPRS and your Sim Card. To check your APN you could type: AT+CSTT...
by Jacket Chen
Thu May 07, 2015 11:41 am
Forum: Arduino & Seeeduino
Topic: Arduino Studio 1.6.3 with Xadow?
Replies: 4
Views: 2707

Re: Arduino Studio 1.6.3 with Xadow?

Thanks for your sharing, i have added it to the wiki of Xadow - Main board.

Jacket
by Jacket Chen
Wed May 06, 2015 11:53 am
Forum: Arduino & Seeeduino
Topic: Stalker V3 wiki isn't consistent on RTC libraries
Replies: 4
Views: 3432

Re: Stalker V3 wiki isn't consistent on RTC libraries

Hi

The library of DS1337 which downloaded from wiki can work well with stalker. You can download the attachment and have a try again.

By the way, did you put the library into a right path? Errors like that always occurred by a wrong path.

Jacket
by Jacket Chen
Wed May 06, 2015 11:43 am
Forum: Arduino & Seeeduino
Topic: newbie problem with knob
Replies: 1
Views: 1389

Re: newbie problem with knob

Hi

Code: Select all

int test_value = knob_level;
try to delete int.

Code: Select all

test_value = knob_level;
Jacket
by Jacket Chen
Tue May 05, 2015 9:44 am
Forum: Grove
Topic: Grove - FM Receiver
Replies: 4
Views: 2027

Re: Grove - FM Receiver

A few more questions . . . Can the FM receiver be used standalone, without any other boards (as long as it is connected to power)? And in this case, is it possible to tune the station directly on the board, or do I need to attach an external potentiometer? Will the board retain the previous station...
by Jacket Chen
Thu Apr 30, 2015 4:46 pm
Forum: Arduino & Seeeduino
Topic: Rainbowduino 3.0 code for Rainbow cube Help...
Replies: 1
Views: 1236

Re: Rainbowduino 3.0 code for Rainbow cube Help...

Please download this attachment and have a try. And show more details to me if you still have this issue.

Jacket
by Jacket Chen
Thu Apr 30, 2015 4:44 pm
Forum: Arduino & Seeeduino
Topic: Simple webserver with Wifi Shield
Replies: 7
Views: 5847

Re: Simple webserver with Wifi Shield

I have watched the video https://www.youtube.com/watch?v=ek63patAl80 And I can see that the code works, however, I think that there is some difficulty with the former boards; like I said before, I have the Wifi_Shield_V1.1 which is not the latest board. I have got a message : please make sure your ...