Search found 8 matches

by Surfacing
Sun Sep 02, 2012 12:09 am
Forum: Arduino & Seeeduino
Topic: Mega2560 + Seeedstudio GPRS Sim900
Replies: 1
Views: 2011

Mega2560 + Seeedstudio GPRS Sim900

Hey everyone. My GPRS shield is running (Serial communication). SMS/Phone is allready working. But I'm not able to connect to the internet. Httpaction response with 601 - Network problem. ciicr response: PDP deact. at+cgreg=? -> 0,1,2 The Networksettings are: APN: A1.net Uname: ppp@A1plus.at PW: ppp...
by Surfacing
Wed Aug 29, 2012 10:02 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

Sorry für die lange Pause. Hab das Ganze mal wieder angetestet. Hab jetzt auch mal einen Raw output zusammen gebracht: #include <SoftwareSerial.h> SoftwareSerial GPRS(6,7); void setup() { GPRS.begin(38400); // the GPRS baud rate Serial.begin(38400); // the Serial port of Arduino baud rate. } void lo...
by Surfacing
Thu Jun 07, 2012 8:02 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

Aha ok... Wie mach ich das? Bzw. Mi ist aufgefallen wenn man die Bautrate ändert, kann man mal mehr/mal weniger lesen. Weis jetzt nicht mehr genau, was ich getestet habe aber irgendwas zwischen 9600 und 38400 glaub ich. Aber wenn du den Code ausprobiert, der oben gepostet ist, bekommst du das dann a...
by Surfacing
Tue Jun 05, 2012 11:55 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

schmron, meinst du das .hex file?

hex-file ist im anhang...

Keine ahnung was du mit string in der comm. meinst. Ich send (per hand) garnichts.
Alles andere ist aus dem Demo-Code (Anhang)

Hex:
Bluetooth_Uno.hex.zip
Demo:Code:
Bluetooth_Uno.pde.zip
lg. Danke!
by Surfacing
Sat May 26, 2012 5:40 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

All messages that are sended are listed in my first comment! The code is 1:1 the demo code provided from Seeed Studio. I just added one Serial.println() which is printing: [...] while(1){ if(blueToothSerial.available()){ recvChar = blueToothSerial.read(); Serial.print(recvChar); recvBuf += recvChar;...
by Surfacing
Fri May 25, 2012 4:09 pm
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

Hey. Sure u can.

View

On the Uno, all Pins are used, and yes I've put it in the correct way (one side 5V/GND and other side Digitalpins) xD
by Surfacing
Fri May 25, 2012 3:28 am
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Re: Arduino Uno + BluetoothShield (SLD63030P)

Thx 4 the reply... I actually read that, but it dont work on the Uno . The Mega is used as Slave, it is in inquiring mode (SeeedStudio DemoCode Mega-Slave) The Uno uses the Master code, but as I've written before, the output of search is just weird char's. And if I understand the Code right, it trig...
by Surfacing
Wed May 23, 2012 1:33 am
Forum: Bee series & WSN
Topic: Arduino Uno + BluetoothShield (SLD63030P)
Replies: 11
Views: 8215

Arduino Uno + BluetoothShield (SLD63030P)

Hey everyone! I've got a problem with the BT Shield (SLD63030P) I try to connect my Uno Board with a Mega2560 Board. Both of them got a BT Shield. I'm able to configure the Shield so it is in Inquireing Mode, but that's all. I changed my Code so that I'm able to read, what the BT Shield reads and pr...