Search found 174 matches

by bobtidey
Tue Apr 19, 2016 4:25 pm
Forum: DSO
Topic: Unable to update with DFU v3.11C
Replies: 5
Views: 4076

Re: Unable to update with DFU v3.11C

Read last post of the thread "update of 2.7B with win10'' on this forum.
by bobtidey
Fri Feb 19, 2016 12:06 am
Forum: DSO
Topic: need master code for HW2.72
Replies: 4
Views: 3930

Re: need master code for HW2.72

No problem.
Hopefully you will see reply soon. They are normally fairly responsive to these requests.
by bobtidey
Thu Feb 18, 2016 11:15 pm
Forum: DSO
Topic: need master code for HW2.72
Replies: 4
Views: 3930

Re: need master code for HW2.72

I have requested one there. Will update when they do.
by bobtidey
Tue Feb 16, 2016 6:53 pm
Forum: DSO
Topic: Wildcat 4.4 user guide
Replies: 6
Views: 6170

Re: Wildcat 4.4 user guide

Not really possible as these main scope apps use multiple slots. Standard one uses 2 and Wildcat uses 3.

Just upgrade to Wildcat; you can always reflash the standard one back.

However Wildcat is simple to use and you'll never use the standard one again!
by bobtidey
Thu Feb 04, 2016 9:24 pm
Forum: DSO
Topic: update of 2.7B with win10
Replies: 2
Views: 6697

Re: update of 2.7B with win10

Windows 10 seemed to need a later DFU than was available for the older 2.7 systems to do updates. Although there was mention of a DFU update I suspect that might be sometime never. Previously I had used an older Win 7 machine but found the following method works although obviously a bit more convolu...
by bobtidey
Wed Dec 23, 2015 8:46 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 557969

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

Does the remark about 2.81 apply only to the revised FPGA part? That's what it sounds like

So one can load v5 app OK onto older devices to benefit from the non FPGA bits?
by bobtidey
Mon Nov 16, 2015 12:14 am
Forum: DSO
Topic: Windows 7 firmware update
Replies: 0
Views: 2760

Windows 7 firmware update

Was updating to Wildcat 4.5. Normally I have had no problems doing this from my main machine running Windows 7 even though I have HW 2.72 and an old DFU3.11C My main machine is on Windows 10 now and I expected that not to work as the DFU driver is not compatible with the older loader firmware and I ...
by bobtidey
Fri Mar 13, 2015 5:43 pm
Forum: DSO
Topic: Newbie here in search of Wildcat and Gabonator
Replies: 2
Views: 2834

Re: Newbie here in search of Wildcat and Gabonator

For wildcat look in the main thread here DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes). Wildcat is an offshoot of the original community edition but now has a lot of improvements and functionality of its own. The most posts in that thread have zips for v3.4 and v4.0. The latter has even ...
by bobtidey
Mon Mar 02, 2015 4:34 pm
Forum: DSO
Topic: DS203 quad user interface design
Replies: 102
Views: 124353

Re: DS203 quad user interface design

That assertion message is being generated during the initial part of the software that tries to load the calibration data from a file called CALIB.DAT Either the file is corrupt or maybe more likely there is some issue in the file access because of 2/8 MB compatibility after you sys changes. It migh...
by bobtidey
Fri Feb 27, 2015 6:16 pm
Forum: DSO
Topic: Phase Measurement?
Replies: 1
Views: 1540

Re: Phase Measurement?

Phase is a measurement between two signals and as far as I know that is not provided automatically by any of the software versions. For it to be a static measurement the two signals need to be of the same frequency. A typical example would be an AC power supply voltage and the corresponding AC curre...