Search found 8 matches

by oakkar7
Fri Mar 04, 2016 9:01 pm
Forum: To Be Classified
Topic: Alternate Payment Method
Replies: 3
Views: 10323

Re: Alternate Payment Method

still no option for payment with visa/master.
Paypal still is restricted Myanmar.

:(
How should I get the deal.
by oakkar7
Fri Nov 27, 2015 10:41 pm
Forum: To Be Classified
Topic: Alternate Payment Method
Replies: 3
Views: 10323

Alternate Payment Method

Hi Seeed! I am from Myanmar. Today, I try to buy some items with Black Friday promotions. There is only one option in Payment Method : PayPal. Problem is that PayPal not work with Myanmar IP address because of sanction. We can use only MASTER/VISA debit and prepaid cards for now. Usually, I used to ...
by oakkar7
Wed Nov 25, 2015 5:11 pm
Forum: To Be Classified
Topic: Feedback
Replies: 9
Views: 28008

Re: Feedback

I accidentally add UPDATES and want to delete it in my recipe. Cannot find a setting for delete/edit UPDATES.
How can I do this ??

http://www.seeedstudio.com/recipe/418-f ... mware.html
by oakkar7
Wed Sep 04, 2013 2:10 pm
Forum: Community Resources
Topic: SeeedStudio invites you to do your own ArduinoPhone!
Replies: 5
Views: 24488

Re: SeeedStudio invites you to do your own ArduinoPhone!

Really, I am ongoing with the same project.
Registration time period is too short.
Dear Seeed, pls let more time for next event.
by oakkar7
Wed Sep 04, 2013 1:52 pm
Forum: To Be Classified
Topic: Anti-spam measures
Replies: 17
Views: 38063

Re: Anti-spam measures

Hi Seeed, I try to comment in some blog posts in last previous 6 months. After that, the comments never shown up. I am from Myanmar and I notice that some of my ISP proxy address are in spammer lists such as botscout.com, www.stopforumspam.com, projecthoneypot.org. But please notice that all users a...
by oakkar7
Wed Apr 18, 2012 2:39 pm
Forum: Bee series & WSN
Topic: GPSBee and MAX232 problem
Replies: 5
Views: 4497

Re: GPSBee and MAX232 problem

Hi Yuri, I don't have UartSB but I have FT232RL module (the same chip as UartSB). So, I connect and test with BPSBee+FT232 module+PC and tested with Hyper terminal and U-center also. Both test show only one "$GPTXT,01,01,02,u-blox ag - www.u-blo$GPTXT,01,01,02,u-blox ag - " string simultaneously. Re...
by oakkar7
Mon Apr 16, 2012 6:33 pm
Forum: Bee series & WSN
Topic: GPSBee and MAX232 problem
Replies: 5
Views: 4497

Re: GPSBee and MAX232 problem

Hi yurip, Sorry, I don't get what you said "You can connect to PC serial port directly first." I already tested GPSBee with PC directly (ie: via MAX232). Or directly connect PC serial port with GPSBee module (without MAX232)? Are you kidding me :). And also tested outdoor about 45mins but nothing ch...
by oakkar7
Mon Apr 16, 2012 3:10 pm
Forum: Bee series & WSN
Topic: GPSBee and MAX232 problem
Replies: 5
Views: 4497

GPSBee and MAX232 problem

Dear Seeeds, I got my GPSBee module since several months ago. I tested the module with MAX232, PC and Hyper terminal but no luck. The problem is that the PC terminal shows only repeated strings. like this, http://www.u-blo$GPTXT,01,01,02,u-blox ag - http://www.u-blo$GPTXT,01,01,02,u-blox ag - http:/...